cancel
Showing results for 
Search instead for 
Did you mean: 

"Synchronous Abort" handler, esr 0x96000006, far 0x0

DMårt
Lead

I wonder why this is happening after U-boot has booten up?

It seems that something is NULL.

 

D/TC:? 0 tee_ta_close_session:484 Destroy session

Error: eth1@482c0000 address not set.
D/TC:? 0 tee_ta_init_session_with_context:562 Re-open trusted service a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x3 ptypes 0x3
F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x4 ptypes 0x651
D/TC:? 0 tee_ta_close_session:465 csess 0x821301f0 id 1
D/TC:? 0 tee_ta_close_session:484 Destroy session
No ethernet found.

�7�[r�[999;999H�[6n�8No EFI system partition
No EFI system partition
Failed to persist EFI variables
D/TC:? 0 tee_ta_init_pseudo_ta_session:303 Lookup pseudo TA ab7a617c-b8e7-4d8f-8301-d09b61036b64
D/TC:? 0 tee_ta_init_pseudo_ta_session:315 Open rng.pta
D/TC:? 0 tee_ta_init_pseudo_ta_session:330 rng.pta : ab7a617c-b8e7-4d8f-8301-d09b61036b64
F/TC:? 0 plat_prng_add_jitter_entropy:74 0x1C
D/TC:? 0 tee_ta_close_session:465 csess 0x821301f0 id 1
D/TC:? 0 tee_ta_close_session:484 Destroy session
D/TC:? 0 tee_ta_init_session_with_context:562 Re-open trusted service a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x3 ptypes 0x3
F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x4 ptypes 0x651
D/TC:? 0 tee_ta_close_session:465 csess 0x82130040 id 1
D/TC:? 0 tee_ta_close_session:484 Destroy session
"Synchronous Abort" handler, esr 0x96000006, far 0x0
elr: 00000000840900b4 lr : 0000000084090b24 (reloc)
elr: 00000000fa0b40b4 lr : 00000000fa0b4b24
x0 : 0000000000000000 x1 : 00000000f8005218
x2 : 0000000000000000 x3 : 0000000000000005
x4 : 0000000000000000 x5 : 00000000fa15f14f
x6 : 0000000000000000 x7 : 0000000000000002
x8 : 00000000f8004e90 x9 : fffffffffffffff0
x10: f80051c800000000 x11: f803531000000000
x12: 2e4af5d406e4cfa8 x13: 99c054c75da28d9f
x14: 00000000f8005058 x15: 00000000f8005060
x16: 00000000fa0c3634 x17: 45afd5bf09c54952
x18: 00000000f8021d50 x19: 00000000f805a1b0
x20: 00000000f8073dd0 x21: 0000000000000000
x22: 00000000fa153c34 x23: 00000000f8075e90
x24: 00000000f8035520 x25: 0000000000000000
x26: 0000000000000000 x27: 00000000fa172c6a
x28: 0000000000000000 x29: 00000000f80050e0

Code: aa0103f0 d61f0200 128004a0 d65f03c0 (f9400002) 
Resetting CPU ...

resetting ...
INFO:    PSCI Power Domain Map:
INFO:      Domain Node : Level 4, parent_node 4294967295, State ON (0x0)
INFO:      Domain Node : Level 3, parent_node 0, State ON (0x0)

 Link to my DT for U-boot: https://github.com/DanielMartensson/Watermelon-Wine-1A/tree/linux-testing/watermelon-wine-os%2Flayers%2Fmeta-watermelon-wine%2Fmx%2Fwatermelon-wine-1a%2FCA35%2FDeviceTree%2Fwatermelon-wine-1a%2Fu-boot

I have attached the output log as well.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
1 ACCEPTED SOLUTION

Accepted Solutions
DMårt
Lead

The problem was in U-boot DT.

&ltdc {
	status = "okay";

	/* USER CODE BEGIN ltdc */
	port{
		#address-cells = <1>;
		#size-cells = <0>;
	};
	/* USER CODE END ltdc */
};

 

The solution was to copy the DT from.DK.

&ltdc {
	status = "okay";

	/* USER CODE BEGIN ltdc */
	port{
		#address-cells = <1>;
		#size-cells = <0>;

		ltdc_ep0_out:endpoint@0{
			reg = <0>;
			remote-endpoint = <&dsi_in>;
		};
	};
	/* USER CODE END ltdc */
};

Now Linux is booting!

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

View solution in original post

1 REPLY 1
DMårt
Lead

The problem was in U-boot DT.

&ltdc {
	status = "okay";

	/* USER CODE BEGIN ltdc */
	port{
		#address-cells = <1>;
		#size-cells = <0>;
	};
	/* USER CODE END ltdc */
};

 

The solution was to copy the DT from.DK.

&ltdc {
	status = "okay";

	/* USER CODE BEGIN ltdc */
	port{
		#address-cells = <1>;
		#size-cells = <0>;

		ltdc_ep0_out:endpoint@0{
			reg = <0>;
			remote-endpoint = <&dsi_in>;
		};
	};
	/* USER CODE END ltdc */
};

Now Linux is booting!

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.