2022-09-16 12:38 AM
EVAL BOARD (stm32mp15-ddr.dtsi)
#define DDR_PCFGR_0 0x00010000
#define DDR_PCFGR_1 0x00010001
My Board (TF-A/stm32mp15-mx-dtsi)
#define DDR_PCFGR_0 0x00000000
#define DDR_PCFGR_1 0x00000000Why are these registers different even though I have the same configuration?
Solved! Go to Solution.
2022-09-16 6:55 AM
HI @Gencay ,
Although impact should be very limited (linked to read/write ordering inside the DDR controller), I confirm that the value in official delivery are the recommended one (See also AN5168).
CubeMX generation will be aligned in future versions.
To sum up, both DDR_PCFGR_0 and DDR_PCFGR_1 should be set to 0x00010000
(I assume 0x00010001 in your post is a typo, if not please provide a link where you found this value)
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2022-09-16 6:55 AM
HI @Gencay ,
Although impact should be very limited (linked to read/write ordering inside the DDR controller), I confirm that the value in official delivery are the recommended one (See also AN5168).
CubeMX generation will be aligned in future versions.
To sum up, both DDR_PCFGR_0 and DDR_PCFGR_1 should be set to 0x00010000
(I assume 0x00010001 in your post is a typo, if not please provide a link where you found this value)
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'