cancel
Showing results for 
Search instead for 
Did you mean: 

How can i change the interface RGMII to RMII using CubeMX?

SPark.15
Associate II

Hello Guys

​

Like the subject, I want change the interface RGMII to RMII using CubeMX.

(RealTek-RTL8211EG-VB-CG => Microchip - LAN8720AI-CP)

Based on STM32MP157C-EV1 Code in CubeMX, I changed the Ethernet option from RGMII to RMII as shown in the picture below.

0693W00000D03NZQAZ.png​

And after Code Generating, I applied it to my addon(mx) directory and built it.

(Changed to the code generated by CubeMX.)

   eth1_pins_mx: eth1_mx-0 {
        pins1 {
            pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_REF_CLK */
                     <STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
                     <STM32_PINMUX('G', 13, AF11)>, /* ETH1_TXD0 */
                     <STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
            bias-disable;
            drive-push-pull;
            slew-rate = <1>;
        };
        pins2 {
            pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
            bias-disable;
            drive-push-pull;
            slew-rate = <0>;
        };
        pins3 {
            pinmux = <STM32_PINMUX('A', 7, AF11)>, /* ETH1_CRS_DV */
                     <STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
                     <STM32_PINMUX('C', 5, AF11)>; /* ETH1_RXD1 */
            bias-disable;
        };
        pins4 {
            pinmux = <STM32_PINMUX('B', 11, AF11)>; /* ETH1_TX_EN */
        };
    };
 
    eth1_sleep_pins_mx: eth1_sleep_mx-0 {
        pins {
            pinmux = <STM32_PINMUX('A', 1, ANALOG)>, /* ETH1_REF_CLK */
                     <STM32_PINMUX('A', 2, ANALOG)>, /* ETH1_MDIO */
                     <STM32_PINMUX('A', 7, ANALOG)>, /* ETH1_CRS_DV */
                     <STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_TX_EN */
                     <STM32_PINMUX('C', 1, ANALOG)>, /* ETH1_MDC */
                     <STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RXD0 */
                     <STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RXD1 */
                     <STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_TXD0 */
                     <STM32_PINMUX('G', 14, ANALOG)>; /* ETH1_TXD1 */
        };
    };
 
 
&ethernet0{
    pinctrl-names = "default", "sleep";
    pinctrl-0 = <&eth1_pins_mx>;
    pinctrl-1 = <&eth1_sleep_pins_mx>;
    status = "okay";
 
    /* USER CODE BEGIN ethernet0 */
    phy-mode = "rgmii-id";
    /*phy-mode = "rmii";*/
    max-speed = <1000>;
    phy-handle = <&phy0>;
 
    mdio0{
        #address-cells = <1>; 
        #size-cells = <0>; 
        compatible = "snps,dwmac-mdio";
 
        phy0:ethernet-phy@0{
            reg = <0>; 
        };
    };   
    /* USER CODE END ethernet0 */
};

However, it seems that the ethernet chip is not recognized as shown in the log below.

~# dmesg | grep eth
[    0.000000] psci: probing for conduit method from DT.
[    1.236408] usbcore: registered new interface driver cdc_ether
[    2.756520] stm32-dwmac 5800a000.ethernet: PTP uses main clock
[    2.760976] stm32-dwmac 5800a000.ethernet: no reset control found
[    2.767028] stm32-dwmac 5800a000.ethernet: No phy clock provided...
[    2.773905] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42
[    2.780299] stm32-dwmac 5800a000.ethernet:   DWMAC4/5
[    2.785190] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported
[    2.792527] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported
[    2.799835] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported
[    2.806696] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported
[    2.812984] stm32-dwmac 5800a000.ethernet: TSO supported
[    2.818278] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[    2.826149] stm32-dwmac 5800a000.ethernet: device MAC address be:10:95:ec:a0:c7
[    2.833449] stm32-dwmac 5800a000.ethernet: TSO feature enabled
[   10.455282] stm32-dwmac 5800a000.ethernet eth0: no phy at addr -1
[   10.475335] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Cannot attach to PHY (error: -19)

I have no experience changing ethernet ICs so I need your help.

​If necessary, I can attach the ethernet circuit diagram of my board.

​

Thanks​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi,

please have a look to AN5031 and https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration#DT_configuration_examples_at_board_level

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
PatrickF
ST Employee

Hi,

please have a look to AN5031 and https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration#DT_configuration_examples_at_board_level

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thank you for your answer.

​In my case I think it's 3.3.1 from your link.

So I applied the line below to the dts file in my addons/mx/PROJECT/u-boot and kernel directory.

    ethernet0: ethernet@5800a000 {
        compatible = "st,stm32mp1-dwmac", "snps,dwmac-4.20a";
        reg = <0x5800a000 0x2000>;
        reg-names = "stmmaceth";
        interrupts-extended = <&intc GIC_SPI 61 IRQ_TYPE_LEVEL_HIGH>,
                              <&intc GIC_SPI 62 IRQ_TYPE_LEVEL_HIGH>,
                              <&exti 70 1>;
        interrupt-names = "macirq",
                          "eth_wake_irq",
                          "stm32_pwr_wakeup";
        clock-names = "stmmaceth",
                      "mac-clk-tx",
                      "mac-clk-rx",
                      "ethstp";
        clock = <&rcc ETHMAC>,
                <&rcc ETHTX>,
                <&rcc ETHRX>,
                <&rcc ETHSTP>;
        st,syscon = <&syscfg 0x4>;
        snps,mixed-burst;
        snps,pbl = <2>; 
        snps,en-tx-lpi-clockgating;
        snps,axi-config = <&stmmac_axi_config_0>;
        snps,tso;
        power-domains = <&pd_core>;
        status = "disabled";
    }; 

After that, an error occurs when bitbake. Do I need to apply it to a file other than the one in that location?

Hi,

I'm more HW oriented, so I cannot help much on SW aspects.

Have you carefully followed the steps in https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package ?

This could also help:

https://wiki.st.com/stm32mpu/wiki/How_to_create_your_board_device_tree

https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

HI !

I solved that problem.

It was a HW problem, not a BSP problem.

But your answer helped me find my HW problem.

Thank you very much!