cancel
Showing results for 
Search instead for 
Did you mean: 

OCTOSPI 256MB errata clarification (is NAND affected?)

Martin Devera
Associate III

There is official errata named "2.5.6 Indirect write mode limited to 256 Mbytes" where indirect OSPI write requests for addr >256MB are written to invalid target address. I tested the behavior and it seems address is effectively truncated to 28bits. Contrary to what errata says, I can see the same truncated address also for indirect reads.

From what I see the problem is affecting NORs only because NAND uses page addressing in 0x13/0x10 cmds and these are always smaller than 24bits.

Is the assumption correct ?

Martin

0 REPLIES 0