cancel
Showing results for 
Search instead for 
Did you mean: 

Yocto Kirkstone stm32mp157f TF_A_CONFG[trusted] not getting generated

gauravpathak
Associate

I am using Yocto build for stm32mp157f. I am following oe-manifest/default.xml at kirkstone · STMicroelectronics/oe-manifest (github.com).
I am able to generate a build, however, I would like to generate tf-a-stm32mp157f-dk2-trusted.stm32 and u-boot-stm32mp157f-dk2-trusted.stm32 which is not getting generated during the build.

The contents of final build are shown below:

tmp-glibc/work/stm32mp15_disco-ostl-linux-gnueabi/tf-a-stm32mp/v2.6-stm32mp-r2.1-r0/deploy-tf-a-stm32mp ├── arm-trusted-firmware │ ├── debug │ │ ├── debug-tf-a-stm32mp157f-dk2-sdcard.stm32 │ │ ├── debug-tf-a-stm32mp157f-dk2-uart.stm32 │ │ ├── debug-tf-a-stm32mp157f-dk2-usb.stm32 │ │ ├── tf-a-bl2-sdcard.elf │ │ ├── tf-a-bl2-uart.elf │ │ └── tf-a-bl2-usb.elf │ ├── fwconfig │ │ └── stm32mp157f-dk2-fw-config-optee.dtb │ ├── metadata.bin │ ├── tf-a-stm32mp157f-dk2-sdcard.stm32 │ ├── tf-a-stm32mp157f-dk2-uart.stm32 │ └── tf-a-stm32mp157f-dk2-usb.stm32 └── fip └── fip-stm32mp157f-dk2-optee.bin

I would like to know what configuration do I need to make to generate tf-a-stm32mp157f-dk2-trusted.stm32 and u-boot-stm32mp157f-dk2-trusted.stm32.
I used below command for setting Yocto environment.
DISTRO=openstlinux-weston MACHINE=stm32mp15-disco source layers/meta-st/scripts/envsetup.sh

bitbake st-image-core

1 REPLY 1
Billy OWEN
ST Employee

Hi @gauravpathak 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy