cancel
Showing results for 
Search instead for 
Did you mean: 

wifi enabling problem

asadullah4571
Senior

hi 
i successfully connecting wifi on STM32mp157f-DK2 board through IPhone but the when i pass the command 

"# ping google.com " then it show temporary failure  in name resolution ,  and also dhcp command not found why this is happen. please reach me out As soon as possible

 

1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi, just tested on STM32MP157x-DK2 with the https://wiki.st.com/stm32mpu/wiki/How_to_setup_a_WLAN_connection#Automatic_WiFi_configuration_at_start_up

(only section 3 to be followed).

No issue to ping google.com (using Android phone as hotspot)

Tested after sync + reboot and also after a complete power down. No issue, connection is still automatic and working.

root@stm32mp1:~# ifconfig wlan0
wlan0     Link encap:Ethernet  HWaddr 00:9D:6B:87:40:FB
          inet addr:192.168.43.202  Bcast:192.168.43.255  Mask:255.255.255.0
          inet6 addr: fe80::29d:6bff:fe87:40fb/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:35 errors:0 dropped:0 overruns:0 frame:0
          TX packets:76 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:4837 (4.7 KiB)  TX bytes:10701 (10.4 KiB)


root@stm32mp1:~# cat /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
ctrl_interface=/var/run/wpa_supplicant
eapol_version=1
ap_scan=1
fast_reauth=1

network={
        psk=b73eb99d9bb4e249def63d24177ca0d51ae9baa96306e0aeed87c063cf44b4e8
}


root@stm32mp1:~# iw wlan0 link
Connected to 4e:6a:f7:b4:f5:e4 (on wlan0)
        SSID: xxxxxxx
        freq: 2437
        RX: 6726 bytes (35 packets)
        TX: 12767 bytes (73 packets)
        signal: -30 dBm
        rx bitrate: 1.0 MBit/s
        tx bitrate: 24.0 MBit/s

        bss flags:      short-preamble short-slot-time
        dtim period:    2
        beacon int:     100


root@stm32mp1:~# ping google.com
PING google.com (216.58.213.78) 56(84) bytes of data.
64 bytes from lhr25s01-in-f78.1e100.net (216.58.213.78): icmp_seq=1 ttl=113 time=59.6 ms

 

Did you have anything to share like above to see some error messages  ?

Is timedatectl show synchronized data/time ?

On my side, the "temporary failure  in name resolution" appear when I shutdown the wifi hotspot on the phone (so, you are likely not really connected to your iPhone hotspot).

 

Maybe start again the setup from a fresh Starter Package of Ecosystem v5.1.0

 

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

View solution in original post

10 REPLIES 10
PatrickF
ST Employee

Hi @asadullah4571 

this might be due to some security on the phone or the board date/time not aligned (as there is no RTC battery on the board).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
Andrew Neil
Super User

@asadullah4571 wrote:

connecting wifi ... through IPhone


You mean using the iPhone as a "hotspot"?

Does this work with any other devices?

ie, as @PatrickF suggested, how do you know it's not just an issue with the iPhone?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

yes you are right, there is no RTC connection, 
but my IPhone hostpot is connected but i need to find the ip address but there is no ip found(IPV4), only i can see the IPV6, and why dhclient command not found. i have to do  manually add the ip address and default gatway.

and the second question why it is not connected automatic once i add the SSID and Password. only iphone is connected i tryied with Android but not connected  

yes i am using iphone as a hotspot
No i tried many time with different different Android phone and also router but not connected i am facing this issue still now 

Hi,

did you use this wiki page ?
https://wiki.st.com/stm32mpu/index.php?title=How_to_setup_a_WLAN_connection&sfr=stm32mpu

 

Did you removed any Ethernet cable on the board (might conflict).

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

@asadullah4571 wrote:

i tried many time with different different Android phone and also router 


I meant can any other devices connect successfully through your iPhone hotspot?

In other words, are you sure that the problem isn't (partly, at least) in your iPhone hotspot?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

yes, i already see the Automatic wifi connection i do that, my iphone hotspot connection is connected but i am triying to use $ping goole.com it will show the tempory unavailable not connected ,

and 1st manually i have to connect the iphone not automatic 

 

yes other devices can connect iphone hotspot easily 

i am facing the issue after connecting wifi form iPhone hotspot so but ip address i have to add manually why and $ dhclient wlan0  it will show the dhclient not found why?? 

PatrickF
ST Employee

Hi, just tested on STM32MP157x-DK2 with the https://wiki.st.com/stm32mpu/wiki/How_to_setup_a_WLAN_connection#Automatic_WiFi_configuration_at_start_up

(only section 3 to be followed).

No issue to ping google.com (using Android phone as hotspot)

Tested after sync + reboot and also after a complete power down. No issue, connection is still automatic and working.

root@stm32mp1:~# ifconfig wlan0
wlan0     Link encap:Ethernet  HWaddr 00:9D:6B:87:40:FB
          inet addr:192.168.43.202  Bcast:192.168.43.255  Mask:255.255.255.0
          inet6 addr: fe80::29d:6bff:fe87:40fb/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:35 errors:0 dropped:0 overruns:0 frame:0
          TX packets:76 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:4837 (4.7 KiB)  TX bytes:10701 (10.4 KiB)


root@stm32mp1:~# cat /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
ctrl_interface=/var/run/wpa_supplicant
eapol_version=1
ap_scan=1
fast_reauth=1

network={
        psk=b73eb99d9bb4e249def63d24177ca0d51ae9baa96306e0aeed87c063cf44b4e8
}


root@stm32mp1:~# iw wlan0 link
Connected to 4e:6a:f7:b4:f5:e4 (on wlan0)
        SSID: xxxxxxx
        freq: 2437
        RX: 6726 bytes (35 packets)
        TX: 12767 bytes (73 packets)
        signal: -30 dBm
        rx bitrate: 1.0 MBit/s
        tx bitrate: 24.0 MBit/s

        bss flags:      short-preamble short-slot-time
        dtim period:    2
        beacon int:     100


root@stm32mp1:~# ping google.com
PING google.com (216.58.213.78) 56(84) bytes of data.
64 bytes from lhr25s01-in-f78.1e100.net (216.58.213.78): icmp_seq=1 ttl=113 time=59.6 ms

 

Did you have anything to share like above to see some error messages  ?

Is timedatectl show synchronized data/time ?

On my side, the "temporary failure  in name resolution" appear when I shutdown the wifi hotspot on the phone (so, you are likely not really connected to your iPhone hotspot).

 

Maybe start again the setup from a fresh Starter Package of Ecosystem v5.1.0

 

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here