2024-08-21 4:24 PM - edited 2024-08-26 3:54 AM
I have compiled tf-a, optee, kernel and u-boot inside STM32CubeIDE.
I have copy over the uImage from the linux build/arch/arm/boot/ and the .dtb file as well. They have been copied over to st-image-bootfs-openstlinux-weston-stm32mp1.ext4 file. I'm only changing the st-image-bootfs-openstlinux-weston-stm32mp1.ext4 file from the Starter Package form STM32MP1 series. The rest e.g st-image-weston-openstlinux-weston-stm32mp1.ext4, st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 and st-image-userfs-openstlinux-weston-stm32mp1.ext4 are not changed.
The kernel is booting, no problem there. But the login promt does not appear. It seems that I got no errors at all, when I look at the full log. My thoughts is that what if bootfs not booting up the software such as command prompt?
The last snippet of the kernel boot log from UART4.
D/TC:0 pwr_scv_handler:56 PWR service: set 0x40000000 at offset 0xc
D/TC:0 pwr_scv_handler:56 PWR service: set 0x10000000 at offset 0xc
D/TC:0 pwr_scv_handler:56 PWR service: clear 0x10000000 at offset 0xc
D/TC:0 pwr_scv_handler:56 PWR service: clear 0x40000000 at offset 0xc
[ 4.151879] stm32-usbphyc 5a006000.usbphyc: registered rev:1.0
[ 4.164077] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0
[ 4.172909] dwc2 49000000.usb-otg: supply vusb_d not found, using dummy regulator
[ 4.179380] dwc2 49000000.usb-otg: supply vusb_a not found, using dummy regulator
D/TC:0 pwr_scv_handler:56 PWR service: set 0x40000000 at offset 0xc
D/TC:0 pwr_scv_handler:56 PWR service: set 0x10000000 at offset 0xc
[ 4.202023] dwc2 49000000.usb-otg: EPs: 9, dedicated fifos, 952 entries in SPRAM
D/TC:0 pwr_scv_handler:56 PWR service: clear 0x10000000 at offset 0xc
D/TC:0 pwr_scv_handler:56 PWR service: clear 0x40000000 at offset 0xc
D/TC:0 pwr_scv_handler:56 PWR service: set 0x40000000 at offset 0xc
D/TC:0 pwr_scv_handler:56 PWR service: set 0x10000000 at offset 0xc
[ 4.241950] ohci-platform 5800c000.usb: Generic Platform OHCI controller
[ 4.247661] ohci-platform 5800c000.usb: new USB bus registered, assigned bus number 1
[ 4.255209] ehci-platform 5800d000.usb: EHCI Host Controller
[ 4.260801] ehci-platform 5800d000.usb: new USB bus registered, assigned bus number 2
[ 4.269000] ohci-platform 5800c000.usb: irq 53, io mem 0x5800c000
[ 4.275225] ehci-platform 5800d000.usb: irq 52, io mem 0x5800d000
[ 4.287751] mmc0: new DDR MMC card at address 0001
[ 4.292389] mmcblk0: mmc0:0001 008GB0 7.28 GiB
[ 4.304665] ehci-platform 5800d000.usb: USB 2.0 started, EHCI 1.00
[ 4.310916] hub 2-0:1.0: USB hub found
[ 4.313642] hub 2-0:1.0: 2 ports detected
[ 4.317706] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9
[ 4.327652] mmcblk0boot0: mmc0:0001 008GB0 4.00 MiB
[ 4.333975] mmcblk0boot1: mmc0:0001 008GB0 4.00 MiB
[ 4.340047] mmcblk0rpmb: mmc0:0001 008GB0 4.00 MiB, chardev (244:0)
[ 4.350948] hub 1-0:1.0: USB hub found
[ 4.353356] hub 1-0:1.0: 2 ports detected
This is my FlasLayout for flashing the eMMC.
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-usb.stm32
- 0x03 fip-boot FIP none 0x0 fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
P 0x04 fsbl1 Binary mmc0 boot1 arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P 0x05 fsbl2 Binary mmc0 boot2 arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P 0x06 metadata1 FWU_MDATA mmc0 0x00080000 arm-trusted-firmware/metadata.bin
P 0x07 metadata2 FWU_MDATA mmc0 0x00100000 arm-trusted-firmware/metadata.bin
P 0x08 fip-a FIP mmc0 0x00180000 fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
PED 0x09 fip-b FIP mmc0 0x00580000 none
PED 0x0A u-boot-env ENV mmc0 0x00980000 none
P 0x10 bootfs System mmc0 0x00A00000 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P 0x11 vendorfs FileSystem mmc0 0x04A00000 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P 0x12 rootfs FileSystem mmc0 0x05A00000 st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x13 userfs FileSystem mmc0 0x33A00000 st-image-userfs-openstlinux-weston-stm32mp1.ext4
Promt from U-boot
STM32MP> mmc part
Partition Map for MMC device 0 -- Partition Type: EFI
Part Start LBA End LBA Name
Attributes
Type GUID
Partition GUID
1 0x00000400 0x000007ff "metadata1"
attrs: 0x0000000000000000
type: 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23
(8a7a84a0-8387-40f6-ab41-a8b9a5a60d23)
guid: df1c26fd-a193-41e9-bb1d-ceb52b8f49ba
2 0x00000800 0x00000bff "metadata2"
attrs: 0x0000000000000000
type: 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23
(8a7a84a0-8387-40f6-ab41-a8b9a5a60d23)
guid: bd11de64-e9bb-457b-9d4a-b75987fe62ae
3 0x00000c00 0x00002bff "fip-a"
attrs: 0x0000000000000000
type: 19d5df83-11b0-457b-be2c-7559c13142a5
(19d5df83-11b0-457b-be2c-7559c13142a5)
guid: 4fd84c93-54ef-463f-a7ef-ae25ff887087
4 0x00002c00 0x00004bff "fip-b"
attrs: 0x0000000000000000
type: 19d5df83-11b0-457b-be2c-7559c13142a5
(19d5df83-11b0-457b-be2c-7559c13142a5)
guid: 09c54952-d5bf-45af-acee-335303766fb3
5 0x00004c00 0x00004fff "u-boot-env"
attrs: 0x0000000000000000
type: 3de21764-95bd-54bd-a5c3-4abe786f38a8
(u-boot-env)
guid: 1c380e98-da64-4fbe-88b4-a516167ea0a7
6 0x00005000 0x00024fff "bootfs"
attrs: 0x0000000000000004
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: ab4be8bf-456c-4365-98cb-c21f48e19c92
7 0x00025000 0x0002cfff "vendorfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: 8d2075a7-dfa6-446f-8852-c89e0819a204
8 0x0002d000 0x0019cfff "rootfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: e91c4e10-16e6-4c0e-bd0e-77becf4a3582
9 0x0019d000 0x00e8fbff "userfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: 5ff28c0a-bc5f-4c0c-b116-a87c0221a7b2
STM32MP>
So what should it stand here? I have tried mmcblk0p8 (the rootfs partition) without success.
# Generic Distro Configuration file generated by OpenEmbedded
MENU BACKGROUND /splash_landscape.bmp
TIMEOUT 20
LABEL OpenSTLinux
KERNEL /uImage
FDTDIR /
INITRD /st-image-resize-initrd
APPEND root=/dev/<what should it be here?> rootwait rw console=${console},${baudrate} loglevel=7
Update:
It seems that the U-boot can read the eMMC very properly without any issues.
STM32MP> ext4ls mmc 0:8 /
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 16384 lost+found
<DIR> 4096 bin
<DIR> 4096 boot
<DIR> 4096 dev
<DIR> 4096 etc
<DIR> 4096 home
<DIR> 4096 lib
<DIR> 4096 media
<DIR> 4096 mnt
<DIR> 4096 proc
<DIR> 4096 run
<DIR> 4096 sbin
<DIR> 4096 srv
<DIR> 4096 sys
<DIR> 4096 tmp
<DIR> 4096 usr
<DIR> 4096 var
<DIR> 4096 vendor
STM32MP> mmc part
Partition Map for MMC device 0 -- Partition Type: EFI
Part Start LBA End LBA Name
Attributes
Type GUID
Partition GUID
1 0x00000400 0x000007ff "metadata1"
attrs: 0x0000000000000000
type: 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23
(8a7a84a0-8387-40f6-ab41-a8b9a5a60d23)
guid: 7c9ee4f6-c9b1-4ec0-b2c4-84d8db334642
2 0x00000800 0x00000bff "metadata2"
attrs: 0x0000000000000000
type: 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23
(8a7a84a0-8387-40f6-ab41-a8b9a5a60d23)
guid: 397e6b52-0f5d-4488-ad25-3273e24a6cc4
3 0x00000c00 0x00002bff "fip-a"
attrs: 0x0000000000000000
type: 19d5df83-11b0-457b-be2c-7559c13142a5
(19d5df83-11b0-457b-be2c-7559c13142a5)
guid: 4fd84c93-54ef-463f-a7ef-ae25ff887087
4 0x00002c00 0x00004bff "fip-b"
attrs: 0x0000000000000000
type: 19d5df83-11b0-457b-be2c-7559c13142a5
(19d5df83-11b0-457b-be2c-7559c13142a5)
guid: 09c54952-d5bf-45af-acee-335303766fb3
5 0x00004c00 0x00004fff "u-boot-env"
attrs: 0x0000000000000000
type: 3de21764-95bd-54bd-a5c3-4abe786f38a8
(u-boot-env)
guid: 70a63b54-4a77-433e-bffc-e9454419b234
6 0x00005000 0x00024fff "bootfs"
attrs: 0x0000000000000004
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: 645715cb-9814-455e-933c-9b7633de2b31
7 0x00025000 0x0002cfff "vendorfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: ee245663-6b56-4d5e-b3c6-797aec6a4f15
8 0x0002d000 0x0019cfff "rootfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: e91c4e10-16e6-4c0e-bd0e-77becf4a3582
9 0x0019d000 0x00e8fbff "userfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: b9f750e0-aab5-422a-b9b0-1ee0d9f430f6
STM32MP> mmc info
Device: STM32 SD/MMC
Manufacturer ID: 11
OEM: 0
Name: 008GB0
Bus Speed: 52000000
Mode: MMC High Speed (52MHz)
Rd Block Len: 512
MMC version 5.1
High Capacity: Yes
Capacity: 7.3 GiB
Bus Width: 8-bit
Erase Group Size: 512 KiB
HC WP Group Size: 4 MiB
User Capacity: 7.3 GiB WRREL
Boot Capacity: 4 MiB ENH
RPMB Capacity: 4 MiB ENH
Boot area 0 is not write protected
Boot area 1 is not write protected
STM32MP> ext4ls mmc 0:8 /sbin
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 4096 .debug
42992 agetty
<SYM> 19 arp
18072 badblocks
<SYM> 22 blkid
71844 blkid.util-linux
<SYM> 25 blockdev
42896 blockdev.util-linux
91156 bridge
68208 cfdisk
3581 check-gpu
22252 ctrlaltdel
137980 debugfs
<SYM> 17 depmod
<SYM> 11 depmod.kmod
22308 dumpe2fs
9780 e2freefrag
232568 e2fsck
232568 fsck.ext2
232568 fsck.ext3
232568 fsck.ext4
38864 e2image
22308 e2mmpstatus
13928 e2undo
13908 e4crypt
22136 e4defrag
<SYM> 22 fdisk
97000 fdisk.util-linux
13840 filefrag
<SYM> 21 fsck
34768 fsck.util-linux
<SYM> 23 fstrim
43020 fstrim.util-linux
<SYM> 12 getty
<SYM> 14 halt
<SYM> 19 hdparm
92924 hdparm.hdparm
<SYM> 24 hwclock
51164 hwclock.util-linux
<SYM> 19 ifconfig
<SYM> 19 ifdown
<SYM> 19 ifup
<SYM> 22 init
<SYM> 17 insmod
<SYM> 11 insmod.kmod
<SYM> 17 ip
454560 ip.iproute2
<SYM> 19 klogd
489044 ldconfig
<SYM> 19 loadkmap
<SYM> 19 logread
9756 logsave
<SYM> 24 losetup
67668 losetup.util-linux
<SYM> 15 lsmod
<SYM> 19 mdev
<SYM> 22 mke2fs
96760 mke2fs.e2fsprogs
96760 mkfs.ext2.e2fsprogs
96760 mkfs.ext3
96760 mkfs.ext4
<SYM> 25 mkfs.ext2
5612 mklost+found
<SYM> 23 mkswap
67612 mkswap.util-linux
<SYM> 18 modinfo
<SYM> 11 modinfo.kmod
<SYM> 19 modprobe
<SYM> 11 modprobe.kmod
2387 mount-copybind
4304 mount-partitions.sh
<SYM> 20 nologin
5580 nologin.shadow
9808 nologin.util-linux
<SYM> 27 pivot_root
9740 pivot_root.util-linux
2460 populate-extfs.sh
<SYM> 14 poweroff
<SYM> 14 reboot
3238 resize-helper
47136 resize2fs
<SYM> 21 resolvconf
<SYM> 16 rmmod
<SYM> 11 rmmod.kmod
<SYM> 19 route
66500 rtmon
<SYM> 14 runlevel
<SYM> 19 setconsole
<SYM> 14 shutdown
484 shutdown-stm32mp1-m4.sh
2080 st-m4firmware-load-default.sh
4364 stm32_usbotg_eth_config.sh
261 stm32mp-coredump-sysfs.sh
<SYM> 24 sulogin
34704 sulogin.util-linux
<SYM> 24 swapoff
13964 swapoff.util-linux
<SYM> 23 swapon
34700 swapon.util-linux
<SYM> 28 switch_root
9804 switch_root.util-linux
<SYM> 19 sysctl
18044 sysctl.procps
<SYM> 19 syslogd
<SYM> 16 telinit
<SYM> 12 udevadm
<SYM> 26 udevd
<SYM> 19 udhcpc
4260 userfs-cleanup-package.sh
<SYM> 17 vigr
<SYM> 11 vigr.shadow
<SYM> 17 vipw
35768 vipw.shadow
<SYM> 19 watchdog
STM32MP>
Solved! Go to Solution.
2024-09-06 2:06 AM
Hi @DMårt
Reading Working custom board for STM32MP151 - Found the so... - STMicroelectronics Community I understand you might have solved this issue by yourself right ?
Can you share solution ?
Thx
Olivier
2024-09-06 2:06 AM
Hi @DMårt
Reading Working custom board for STM32MP151 - Found the so... - STMicroelectronics Community I understand you might have solved this issue by yourself right ?
Can you share solution ?
Thx
Olivier
2024-09-06 11:02 AM
My solution is to NOT destroy the working queue for STM32MP151 series. Then everything will work. Ethernet, USB, HDMI, eMMC, PMIC.
I think the best way for ST is to build my custom bord and try it. ST can learn alot of it.
There are alot of custom boards of STM32P151 series, but non of them seems to work, from what I have seen in this forum.