2024-10-19 4:39 AM
Hi ST Team ,
previously i used the MP1 processor where the video lagging issues, so know i decided to move on another processor who can play the high resolution video above 1080 P @30FPS,
Note: i do not want any HDMI IC's , i want direct pin(RGB) through the processor to our HDMI port,
please suggest me which Processor should be better.
2024-10-20 11:28 PM
STM32MP2 series are able to play 1080p60 thru LTDC in RGB (depending on blanking required).
Note that ~150MHz clock with 24 bits RGB parallel data bus is challenging in term of general power noise and signal integrity. LTDC bus must be very short and with very low capacitive load.
We recommend to use DSI which could go up to 2048 × 1536 60 fps with much less pins and far much easier signal integrity as using low voltage differential pairs.
On STM32MP257F-DK board, we provide 1080p60 HDMI using the onboard DSI2HDMI converter (ADV7535BCBZ).
Regards
2024-10-28 3:42 AM
Hi @PatrickF
I am making the project on STM32mp257 board, as you suggested but i want to know form your side that, will it support for Chromium browser or Firefox?. in your yocto Distribution package there will be no issues with font decoding and as well as video playing.
2024-10-28 3:54 AM
Hi,
I don't know, MPUs product with embedded Linux are not focusing to be used with 'PC-like' browsers. You could evaluate on your side using STM32MP257F-EV board.
As far as I know, when product has an UI, it is usually done using Weston/Wayland/Gtk or Qt.
Regards.
2024-11-14 2:06 AM - edited 2024-11-14 2:10 AM
Hi @PatrickF
I added the 3rd party layers meta-browser with x11 for MP1 board, it works and when i try to play the youtube video, it works but so much lagging issue. So i decided to move on MP2
Now I am going to purchase MP2- DK or EV board, but it should be play youtube video minimum 1080@60 without any lagging issue using DSI2HDMI converter . and i will use 2GB RAM DDR4.
please suggest me will it works?
2024-11-20 3:52 AM
I want to use MP2 as a simple notebook.
Any progress about youtube on the MP2-dev board?
Looking forward for your reply!
2024-11-20 4:10 AM
2024-11-20 4:39 AM
@Andrew Neil yes i know.
I'm just looking for a reply from @asadullah4571
2024-11-20 5:02 AM
You know, but others in this thread might not have seen your other threads on the same topic
2024-11-21 2:55 AM - edited 2024-11-21 2:56 AM
hi @DMårt
Actually i done this on MP1 processor and works fine, becouse of the same branch "krikstone" will support on MP1 as well as Meta-browser.
and I try to build the krikstone branch with MP2 i got the error. "machine target not found". so simply not possible to add meta-browser layer into the Distro package.