2022-07-28 7:05 AM
Hi, and yet another question...
We would like to perform electrical compliance testing on our USB ports. This requires each port to send a test pattern.
Our board has one upstream and two downstream facing ports. The upstream port can be set into various test modes using a standard tool (USB xHSETT). Unfortunately, this is not possible for the downstream ports.
Can you give me any advice, how to set a usb host port into the TEST_PACKET test mode?
Regards
Solved! Go to Solution.
2022-07-28 11:32 PM
Hi @jvog.sen ,
If I got your question I guess you need to set CONFIG_USB_EHSET_TEST_FIXTURE in your kernel.
This configuration enables the ehset driver which is loaded when plugging PIDVID test fixture or USBHSET https://elixir.bootlin.com/linux/latest/source/drivers/usb/misc/ehset.c
which converts PID into USB message to put the controller in the requested test mode.
#define TEST_SE0_NAK_PID 0x0101
#define TEST_J_PID 0x0102
#define TEST_K_PID 0x0103
#define TEST_PACKET_PID 0x0104
#define TEST_HS_HOST_PORT_SUSPEND_RESUME 0x0106
#define TEST_SINGLE_STEP_GET_DEV_DESC 0x0107
#define TEST_SINGLE_STEP_SET_FEATURE 0x0108
Hope it help
Olivier
2022-07-28 11:32 PM
Hi @jvog.sen ,
If I got your question I guess you need to set CONFIG_USB_EHSET_TEST_FIXTURE in your kernel.
This configuration enables the ehset driver which is loaded when plugging PIDVID test fixture or USBHSET https://elixir.bootlin.com/linux/latest/source/drivers/usb/misc/ehset.c
which converts PID into USB message to put the controller in the requested test mode.
#define TEST_SE0_NAK_PID 0x0101
#define TEST_J_PID 0x0102
#define TEST_K_PID 0x0103
#define TEST_PACKET_PID 0x0104
#define TEST_HS_HOST_PORT_SUSPEND_RESUME 0x0106
#define TEST_SINGLE_STEP_GET_DEV_DESC 0x0107
#define TEST_SINGLE_STEP_SET_FEATURE 0x0108
Hope it help
Olivier
2022-07-29 12:32 AM
Hi Olivier,
thanks, that sounds like it could work - I'll give it a shot!
Regards
Jan