2021-06-26 4:01 AM
Hi all,
I am currently using VisionSoM board : STM32MP157AAB3 board.
I am trying to drive an LVDS display via a RGB to LVDS converter.
Here is the datasheet link for it.
The panel settings are as follows :
panel {
u-boot,dm-pre-reloc;
status = "okay";
display-timings {
timing0: timing0 {
clock-frequency = <72400000>;
hactive = <1280>;
vactive = <800>;
hfront-porch = <22>;
hback-porch = <150>;
hsync-len = <160>;
vback-porch = <32>;
vfront-porch = <22>;
vsync-len = <38>;
hsync-active = <0>;
vsync-active = <0>;
de-active = <0>;
pixelclk-active = <1>;
};
};
};
I also modified the driver : panel-simple.c file in kernel/drivers/gpu/drm/panel and added support for this custom display there.
When i run qt demo for playing video on the RGB out i can see on oscilloscope that the clock signal frequency is not going beyond 66.6Mhz .
Earlier I was stuck at clock generation frequency of 33.3Mhz since my changes in device tree were getting ovewritten by the one's in kernel driver since i set the compatible field in device tree to some other display.
But now when i want to generate if for 72.4 Mhz , it is not going beyond 66.6Mhz ?
I am running OpenSTlinux dunfell 5.10 latest version.
Solved! Go to Solution.
2021-06-28 5:34 AM
Hi,
what is your PLL4 frequency (e.g. using "cat /sys/kernel/debug/clk/clk_summary | grep pll4") ?
In Starter Package, the PLL4 frequency is set to 594MHz which mean you can't output precisely 72.4MHz for LTDC pixel clock (pll4_q) with an integer divider (594/72.4 = 8.204...).
Linux will fallback to next possible integer divider (594/9 = 66MHz).
Maybe worth to try using 74.25MHz (594/8) for LTDC pixel clock (this frequency is the one used when we display using LTDC going to HDMI bridge).
See also https://wiki.st.com/stm32mpu/wiki/DRM_KMS_overview.
Regards.
2021-06-28 5:34 AM
Hi,
what is your PLL4 frequency (e.g. using "cat /sys/kernel/debug/clk/clk_summary | grep pll4") ?
In Starter Package, the PLL4 frequency is set to 594MHz which mean you can't output precisely 72.4MHz for LTDC pixel clock (pll4_q) with an integer divider (594/72.4 = 8.204...).
Linux will fallback to next possible integer divider (594/9 = 66MHz).
Maybe worth to try using 74.25MHz (594/8) for LTDC pixel clock (this frequency is the one used when we display using LTDC going to HDMI bridge).
See also https://wiki.st.com/stm32mpu/wiki/DRM_KMS_overview.
Regards.
2021-07-01 10:56 PM
@PatrickF : Thanks a lot for response this really helped.