2025-03-24 7:12 AM
Hello.
I am struggling to get my codec to work. I am using MAX9860 codec.
The MAX9860 driver fails during probing, since the MCLK rate is registered as 0.
I get the following error:
[ 15.465445] max9860 1-0020: Bad mclk 0Hz (needs 10MHz - 60MHz)
[ 15.481832] max9860: probe of 1-0020 failed with error -22
This is the piece of the driver that causes the error:
/*
* mclk has to be in the 10MHz to 60MHz range.
* psclk is used to scale mclk into pclk so that
* pclk is in the 10MHz to 20MHz range.
*/
max9860->mclk_handle = clk_get(dev, "MCLK");
if (IS_ERR(max9860->mclk_handle)) {
ret = PTR_ERR(max9860->mclk_handle);
dev_err_probe(dev, ret, "Failed to get MCLK\n");
goto err_regulator;
}
mclk_rate = clk_get_rate(max9860->mclk_handle);
clk_put(max9860->mclk_handle);
if (mclk_rate > 60000000 || mclk_rate < 10000000) {
dev_err(dev, "Bad mclk %luHz (needs 10MHz - 60MHz)\n",
mclk_rate);
ret = -EINVAL;
goto err_regulator;
}
This is my dts:
/ {
sound {
compatible = "audio-graph-card";
label = "max9860-hifi";
routing =
"Playback", "MCLK",
"Capture", "MCLK";
dais = <&i2s1_port>;
status = "okay";
};
};
&i2c1 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c1_pins_mx>;
pinctrl-1 = <&i2c1_sleep_pins_mx>;
status = "okay";
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
clock-frequency = <100000>;
/delete-property/ dmas;
/delete-property/ dma-names;
max9860: max9860@20 {
compatible = "maxim,max9860";
reg = <0x20>;
AVDD-supply = <&v1v8>;
DVDD-supply = <&v1v8>;
DVDDIO-supply = <&v3v3>;
clocks = <&i2s1>;
clock-names = "MCLK";
codec_port: port {
codec_endpoint: endpoint {
remote-endpoint = <&i2s1_endpoint>;
};
};
};
};
&i2s1 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2s1_pins_mx &i2s1_pins_z_mx>;
pinctrl-1 = <&i2s1_sleep_pins_mx &i2s1_sleep_pins_z_mx>;
status = "okay";
clocks = <&rcc SPI1>, <&rcc SPI1_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "i2sclk", "x8k", "x11k";
#sound-dai-cells = <1>;
#clock-cells = <0>; /* Set I2S1 as master clock provider */
i2s1_port: port {
#address-cells = <1>;
#size-cells = <0>;
i2s1_endpoint: endpoint {
remote-endpoint = <&codec_endpoint>;
format = "i2s";
mclk-fs = <256>;
};
};
};
The clock seems to be properly created, but its rate is 0.
root@stm32mp15-xx:~# cat /sys/kernel/debug/clk/clk_summary | grep mclk
spi1_mclk 0 0 0 0 0 0 50000 ? deviceless no_connection_id
Does anyone know where to look next? Is it most likely a device-tree issue or is it a compatibility issue between ST i2s and the codec driver?
2025-03-28 3:48 AM
Hello @Makandra ,
Could you please activate the dbg traces in stm32_i2s.c file to check the output logs of i2s at probe time and when you try to probe your codec ?
Kind regards,
Erwan.