2020-07-21 5:27 AM
i have following yocto build configuration
Build Configuration:
BB_VERSION = "1.42.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-openstlinux_weston-linux-gnueabi"
DISTRO = "openstlinux-weston"
DISTRO_VERSION = "2.7-snapshot-20200721"
TUNE_FEATURES = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"
TARGET_FPU = "hard"
DISTRO_CODENAME = "warrior"
GCCVERSION = "8.%"
need to what are the simple way to populate /dev/fb0, and draw a simple image RGB888 image , as i have parallel lcd RGB 24 bit display,
dont know what to add in kernel configuration, uboot level
any reference dtsi and more input
would be helpful
2020-07-23 11:55 PM
Hi @Ara.1
First I notice you are using DISTRO_CODENAME = "warrior" which is not a supported distro by ST ( thud or dunfell)
For question about display did you already browse our wiki documentation ?
Guess some page may help you :
https://wiki.st.com/stm32mpu/wiki/DRM_KMS_overview
LTDC device tree configuration and DSI device tree configuration
Hope it help
Olivier
2020-07-29 8:52 PM
Hi Oliver
attached is modtest and necessary log
following is the dts configuration
panel-rgb@0 {
compatible = "okaya,rs800480t-7x0gp", "simple-panel";
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_mp1som_pins_a>;
pinctrl-1 = <<dc_mp1som_sleep_pins_a>;
status = "okay";
port {
panel_in_rgb: endpoint {
remote-endpoint = <<dc_out_rgb>;
};
};
};
/* disable DSI panel */
&dsi {
status = "disabled";
};
<dc {
status = "okay";
port {
ltdc_out_rgb: endpoint@0 {
reg = <0>;
remote-endpoint = <&panel_in_rgb>;
};
};
};
i can able to a white blank screen,
a. simple panel is getting probed successfully
anything else driver or configuration is missing , please let me know
2020-08-03 4:48 AM
attached is the drm log,
please let me know whats happening, still display is not up
2020-09-17 2:50 AM
hi, Olivier GALLIEN
I can display ok by drm with rgb888 lcd on stm32mp153, and "/dev/dri/card0" is ok.
but you know, stm32mp153 don't have gpu
I want running QT on stm32mp153 with "/dev/fb0"
so, how to create the "/dev/fb0"?
I try to modify de devicetree, but it still can't work well
Have you test "/dev/fb0" ok ,before? and how to modify?
thanks
2022-01-12 7:43 AM
There is really no way to use simple framebuffer on mp151/153 devices?
DRM is the only method?
2022-05-29 10:55 PM
Look at CONFIG_DRM_FBDEV_EMULATION kernel build config param