2024-11-20 07:38 AM - edited 2024-11-20 07:39 AM
I modified an FSBL example to get to the root of the problem (everything else being as in the example).
volatile int rrr = 0;
void SGI0_IRQHandler(void) {
while (1) {
rrr++;
};
}
int main()
{
HAL_Init();
SystemClock_Config();
IRQ_Disable(SGI0_IRQn);
IRQ_SetPriority(SGI0_IRQn, 0);
IRQ_Enable(SGI0_IRQn);
while(1) {
GIC_SendSGI(SGI0_IRQn, 1, 0);
}
}
This works perfectly in thumb mode, but when I switch to ARM (that probably should give slight performance boost for my DSP task), the interrupt is stuck in Vectors section, without doing anything.
The LR is weird, and I cant get my head around how is it possible that is has LR = 0x2ffe0106 (not multiple of 4)
As if the core switched to thumb mode without address being odd and started executing instructions in 16 bit mode.
Thanks for any advice :)
2024-11-20 11:56 PM
Hi @bsvi ,
Please confirm you are on baremetal MP13 solution on DK board here ?
Thanks
Olivier
2024-11-21 12:50 AM
Hi @bsvi
you should refer to ARM documents to understand how interrupt are handled.
https://developer.arm.com/documentation/ddi0406/latest/
https://developer.arm.com/documentation/den0013/d/Exception-Handling/Exception-handling
Regards.