cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 interrupt causes undefined exception in ARM mode (but works in thumb)

bsvi
Visitor

I modified an FSBL example to get to the root of the problem (everything else being as in the example).

 

 

 

volatile int rrr = 0;
void SGI0_IRQHandler(void) {
    while (1) {
        rrr++;
    };
}

int main()
{
  HAL_Init();
  SystemClock_Config();

  IRQ_Disable(SGI0_IRQn);

  IRQ_SetPriority(SGI0_IRQn, 0);
  IRQ_Enable(SGI0_IRQn);

  while(1) {
	  GIC_SendSGI(SGI0_IRQn, 1, 0);
  }
}

 

 

 

This works perfectly in thumb mode, but when I switch to ARM (that probably should give slight performance boost for my DSP task), the interrupt is stuck in Vectors section, without doing anything.

bsvi_0-1732116792961.png

The LR is weird, and I cant get my head around how is it possible that is has LR = 0x2ffe0106 (not multiple of 4)

bsvi_1-1732116911656.png

As if the core switched to thumb mode without address being odd and started executing instructions in 16 bit mode.

Thanks for any advice :)

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @bsvi ,

Please confirm you are on baremetal MP13 solution on DK board here ?

Thanks 

Olivier 

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.