2025-01-28 7:33 PM
Hi, I want to use the M4 core to handle all Audio DSP work
I can see that MXCube allows the SAI ports to be enabled on the M4 core
But it appears the I2S ports are not.
I am Missing something here
Unfortunately the Pins I need to be the PZ0-1-2-3 as PCB is done
Else If Its only possible to use the I2S from the Linux A7 then is it even possible to transfer audio data between the cores?
Thanks