STM32MP1 I2S on M4 core
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-01-28 7:33 PM
Hi, I want to use the M4 core to handle all Audio DSP work
I can see that MXCube allows the SAI ports to be enabled on the M4 core
But it appears the I2S ports are not.
I am Missing something here
Unfortunately the Pins I need to be the PZ0-1-2-3 as PCB is done
Else If Its only possible to use the I2S from the Linux A7 then is it even possible to transfer audio data between the cores?
Thanks
Labels:
- Labels:
-
I2S
0 REPLIES 0