2025-01-10 7:45 AM
I've followed the READMEs for the installation of the dev package, source, and kernel and generated a build folder for the kernel as suggested at
~/st/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sdk/Developer-Package/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/aarch64-ostl-linux/linux-stm32mp-6.6.48-stm32mp-r1-r0/build
In the build folder I see folders include, scripts, a link to source as well as files Makefile, .config .config.old, and .gitignore. When I run
make ${IMAGE_KERNEL} vmlinux dtbs LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"
I get
make[1]: *** No rule to make target 'Image.gz'. Stop.
make: *** [/home/lelory/st/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sdk/Developer-Package/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/aarch64-ostl-linux/linux-stm32mp-6.6.48-stm32mp-r1-r0/linux-6.6.48/Makefile:234: __sub-make] Error 2
What am I doing wrong?
Solved! Go to Solution.
2025-01-10 9:11 AM
Hi,
did the SDK correctly installed and the environment sourced ?
Regards.
2025-01-10 9:11 AM
Hi,
did the SDK correctly installed and the environment sourced ?
Regards.
2025-01-10 1:29 PM
Ah, didn't realize I had to source when changing folders as well. Now another issue:
/home/lelory/st/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sdk/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/lib/aarch64-ostl-linux/gcc/aarch64-ostl-linux/13.3.0/plugin/include/builtins.h:23:10: fatal error: mpc.h: No such file or directory
23 | #include <mpc.h>
It doesn't show the file in the gcc and I don't see it there either.