cancel
Showing results for 
Search instead for 
Did you mean: 

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,6)

RBruè.1
Associate II

Hi, I've created a SD card following this guide. The generated SD card partitions can be seen in the screenshot here below. It seems to boot correctly until the kernel prompts the following error:

[    4.200445] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,6) ]---

How to solve this?

Thank you.

0693W00000D0wxrQAB.png

1 ACCEPTED SOLUTION

Accepted Solutions
RBruè.1
Associate II

I've re-written the SD card another time, and now it works as expected, don't sure why it wasn't working before.

View solution in original post

2 REPLIES 2
RBruè.1
Associate II

I've re-written the SD card another time, and now it works as expected, don't sure why it wasn't working before.

Olivier GALLIEN
ST Employee

Hi @Riccardo Bruè​ ,

I will check at my end if there's no problem with the scripts itself.

May you have possibility to program the SDCard on board with STM32CubeProg ?

But this can also come from a wrong uboot configuration.

You have compiled all material with Distri pack right ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.