cancel
Showing results for 
Search instead for 
Did you mean: 

I can not download android starter image to stm32MP1-DK 2 board.

Sergey1
Associate III

I am using starter image "en.st-android-10.0.0-2020-02-21-eval-sd-starter.tar.gz".

CubeProgrammer gave me "Error: an error occurred while uploading data from the virtual partition 0xF1" . Below is full log:

16:56:19 : USB speed : High Speed (480MBit/s)

16:56:19 : Manuf. ID : STMicroelectronics

16:56:19 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

16:56:19 : SN : 0046003E3338510634383330

16:56:19 : FW version : 0x0110

16:56:19 : Device ID : 0x0500

16:56:23 : Start Embedded Flashing service

16:56:23 : Memory Programming ...

16:56:23 : Opening and parsing file: fsbl-programmer.img

16:56:23 : File : fsbl-programmer.img

16:56:23 : Size : 245360 Bytes

16:56:23 : Partition ID : 0x01 

16:56:23 : Download in Progress:

16:56:24 : File download complete

16:56:24 : Time elapsed during download operation: 00:00:00.431

16:56:24 : RUNNING Program ... 

16:56:24 : PartID: :0x01 

16:58:14 : Error: an error occured while uploading data from the virtual partition 0xF1

16:58:14 : Start operation done successfully at partition 0x01

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Nicolas L
ST Employee

Hi @DQays.1​ 

If you need I can provide you sources and directives to allow building the Android 10 delivery for the STM32MP157C-DK2 directly by email.

This solution is just a first integration, not fully validated and clearly not optimized (bad user experience).

Nicolas

View solution in original post

12 REPLIES 12
Olivier GALLIEN
ST Employee

Hi @Sergey​ 

ST-Android delivery only support STM32MP157x-EV1 Evaluation board.

You can't download it on a DK2.

Please refer to :

https://wiki.st.com/stm32mpu/wiki/STM32MP15_distribution_for_Android_release_note_-_v1.1.0

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sergey1
Associate III

Thank you for the answer.

Do you have an example how to modify distribution package for DK2 board?

Or it is not supported by ST?

Thanks.

Olivier GALLIEN
ST Employee

Hi @Sergey​ 

Indeed ST do not support Android on DK2 board because hardware configuration is not appropriate for a correct user experience.

Is it a problem for you to get an EVAL board ?

Thanks

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello,

it is a problem for me to get an EVAL board, because I already have STM32MP157C-DK2.

and as you know, no one like to spend too much money these days.

I know android will be way slow on STM32MP157C-DK2, but that will not be issue for me.

I think a lot of ST customers will be happy if we can power the STM32MP157C-DK2 boards with android.

have a nice day

Qaysaneah

Nicolas L
ST Employee

Hi @DQays.1​ 

If you need I can provide you sources and directives to allow building the Android 10 delivery for the STM32MP157C-DK2 directly by email.

This solution is just a first integration, not fully validated and clearly not optimized (bad user experience).

Nicolas

Hi @Nicolas L​ 

Please send me those sources and directives as well.

Thanks a lot,

Sergey.

Well, We are here because we know that we cannot download it to DK2, but we will see what we can do.

it will be nice to make it less difficult.

have a nice day

Hi @DQays.1​ ,

I'm not sure to understand your today comment.

As explained we don't want to put much effort in providing on-the-shelve solution as we consider as very marginal people that will accept performance on such plateform.

Anyway @Nicolas L​  provided you a private/dedicated support 2 weeks back.

Do you need further ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello

I just see mr @Nicolas L nice email today, I hope all the people like him.

I dont need any further help. at least for now. because I want to follow his instructions and see what come next, ....

thank you anyway and have a nice day