cancel
Showing results for 
Search instead for 
Did you mean: 

I got PANIC at PC : 0x2ffec98b - Why?

DMårt
Lead

I made a custom board with the processor STM32MP151AAC3 and own firmwire https://github.com/DanielMartensson/STM32-Computer/tree/main/STM32CubeIDE/STM32-Computer-Firmware . I have compiled the TF-A by using STM32CubeIDE. It was some bugs with the TF-A configuration, but it seems I fixed them in this thread: 

Solved: BUG: Label or path X_pins_y not found - Compiling ... - STMicroelectronics Community

 

PANIC at PC : 0x2ffec98b

Exception mode=0x00000016 at: 0x2ffec98b

 

I have tried to flash it with firmware of STM32MP157 with another I2C4 pin configuration. And it failed. 

 

NOTICE:  CPU: STM32MP151AAC Rev.Z
NOTICE:  Model: STMicroelectronics STM32MP157A eval daughter on eval mother
ERROR:   I2C device not ready
PANIC at PC : 0x2fff101b

Exception mode=0x00000016 at: 0x2fff101b

Trying the Flashout Delete All DK1 STM32MP157a.
Exception mode=0x00000016 at: 0x2fff101b

NOTICE:  CPU: STM32MP151AAC Rev.Z
NOTICE:  Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
ERROR:   I2C device not ready
PANIC at PC : 0x2fff101b

 

That means the following:

  1. The HSE clock is working
  2. The HSE clock is soldered correctly
  3. The I2C is working, even if it was not ready for communication (wrong pins)

Question:

This new error must lead to an answer. What can it be?

 

 

 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
33 REPLIES 33

@DMårt Thank you. I am trying to understand and solve the USB OTG issue :)

@@5c00a000 device is:

tamp: tamp@5c00a000 {
			compatible = "st,stm32-tamp", "syscon", "simple-mfd";
			#address-cells = <1>;
			#size-cells = <1>;
			reg = <0x5c00a000 0x400>;
			interrupts = <GIC_SPI 197 IRQ_TYPE_LEVEL_HIGH>;
			clocks = <&rcc RTCAPB>;
			ranges;
			st,backup-zones = <10 5 17>;

			nvram: nvram@5c00a100 {
				compatible = "st,stm32mp15-tamp-nvram";
				#address-cells = <1>;
				#size-cells = <1>;
				reg = <0x5c00a100 0x80>;

				wakeup_sec: tamp-bkp@0 {
					reg = <0x0 0x4>;
				};

				m4_security_perimeter_exti1: tamp-bkp@4 {
					/* see cortex-m4 wake up feature */
					reg = <0x4 0x4>;
				};

				m4_security_perimeter_exti2: tamp-bkp@8 {
					/* see cortex-m4 wake up feature */
					reg = <0x8 0x4>;
				};

				m4_security_perimeter_exti3: tamp-bkp@c {
					/* see cortex-m4 wtake up feature */
					reg = <0xc 0x4>;
				};

				magic_number: tamp-bkp@10 {
					/* see ddr and cpu wake up management feature */
					reg = <0x10 0x4>;
				};

				branch_address: tamp-bkp@14 {
					/* see ddr and cpu wake up management feature */
					reg = <0x14 0x4>;
				};

				fwu_info: tamp-bkp@28 {
					/* see firmware update info feature */
					reg = <0x28 0x4>;
				};

				copro_rsc_tbl_address: tamp-bkp@44 {
					/* see cortex-m4 management feature */
					reg = <0x44 0x4>;
				};

				cortex_m_state: tamp-bkp@48 {
					/* see cortex-m4 management feature */
					reg = <0x48 0x4>;
				};

				boot_mode: tamp-bkp@50 {
					/* see boot mode selection feature */
					reg = <0x50 0x4>;
				};

				boot_counter: tamp-bkp@54 {
					/* see boot counter feature */
					reg = <0x54 0x4>;
				};

				m4_wakeup_area_start: tamp-bkp@58 {
					/* see cortex-m4 wake up feature */
					reg = <0x58 0x4>;
				};

				m4_wakeup_area_length: tamp-bkp@5c {
					/* see cortex-m4 wake up feature */
					reg = <0x5c 0x4>;
				};

				m4_wakeup_area_hash: tamp-bkp@60 {
					/* SHA-256 value see Cortex-M4 wake up feature */
					reg = <0x60 0x20>;
				};
			};

			reboot_mode: reboot-mode {
				compatible = "nvmem-reboot-mode";
				nvmem-cells = <&boot_mode>;
				nvmem-cell-names = "reboot-mode";
				mode-normal = <0x00>;
				mode-fastboot = <0x01>;
				mode-recovery = <0x02>;
				mode-stm32cubeprogrammer = <0x03>;
				mode-ums_mmc0 = <0x10>;
				mode-ums_mmc1 = <0x11>;
				mode-ums_mmc2 = <0x12>;
				mode-romcode_serial = <0xff>;
			};
		};

@rgruberski 

Hmm...can you add these to optee?

https://github.com/DanielMartensson/STM32-Computer/blob/827ca34e3cdeb5cbee5c174c85e6c812524328cb/Firmware/STM32-Computer-Firmware/CA7/DeviceTree/STM32-Computer-Firmware/optee-os/stm32mp151a-stm32-computer-firmware-mx.dts#L676

 

Also check out the file "STM32MP15xx-dx.dtsi" in arch/arm/dts folder of optee/tf-a/kernel/u-boot. Very useful examples in there.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

@DMårt I did it, and it changed nothing. Do you mean an arch/arm/dts/stm32mp15xx-dkx? dtsi file?

YEs. Follow that.

But I'm very sure that you got time out when you're connecting

https://github.com/DanielMartensson/STM32-Computer/blob/827ca34e3cdeb5cbee5c174c85e6c812524328cb/Firmware/STM32-Computer-Firmware/CA7/DeviceTree/STM32-Computer-Firmware/tf-a/stm32mp151a-stm32-computer-firmware-mx.dts#L432

 

Copy everything from me. Or else, it's a hardware issue.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer