2024-08-01 8:43 AM - edited 2024-08-01 8:51 AM
I made a custom board with the processor STM32MP151AAC3 and own firmwire https://github.com/DanielMartensson/STM32-Computer/tree/main/STM32CubeIDE/STM32-Computer-Firmware . I have compiled the TF-A by using STM32CubeIDE. It was some bugs with the TF-A configuration, but it seems I fixed them in this thread:
Solved: BUG: Label or path X_pins_y not found - Compiling ... - STMicroelectronics Community
PANIC at PC : 0x2ffec98b
Exception mode=0x00000016 at: 0x2ffec98b
I have tried to flash it with firmware of STM32MP157 with another I2C4 pin configuration. And it failed.
NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157A eval daughter on eval mother
ERROR: I2C device not ready
PANIC at PC : 0x2fff101b
Exception mode=0x00000016 at: 0x2fff101b
Trying the Flashout Delete All DK1 STM32MP157a.
Exception mode=0x00000016 at: 0x2fff101b
NOTICE: CPU: STM32MP151AAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
ERROR: I2C device not ready
PANIC at PC : 0x2fff101b
That means the following:
Question:
This new error must lead to an answer. What can it be?
Solved! Go to Solution.
2024-09-12 1:17 AM
If you're flashing the emmc with the USB OTG, there is a hack you can do to avoid the time out
How does your UART look like when you're reflashing?
What is your BOOT pin configuration when you're flashing?
2024-09-12 1:32 AM
@DMårtThank you!
How does your UART look like when you're reflashing? Please check the attached previous and now file. It's a complete UART log.
What is your BOOT pin configuration when you're flashing? All off (0)
2024-09-12 3:09 AM
The .log file is corrupted. I cannot read it.
ꭀ?⢒?鿈??ꬕ?⯓?⥌?ⱈ?⹋??椐??狙?
2024-09-12 3:11 AM
2024-09-12 3:50 AM
ERROR: nvmem node board_id not found
Det the board ID inside the dts files. See how I did that inside my STM32-Computer repository.
Begin with resolve ALL errors, deffered, and "missing" etc.
It will help.
2024-09-12 4:01 AM
@DMårt Thank you! I have fixed the above error. I can't find errors, deferred, or missing elements in the log file. Have you seen any element I should fix in the log file?
2024-09-12 4:30 AM - edited 2024-09-12 4:31 AM
Are you flashing via USB OTG or SD-card ?
How does your STPMIC look like in the dts file?
2024-09-12 4:36 AM
@DMårt I am flashing via USB OTG on a USB-C connector. This design doesn't include an SD card.
2024-09-12 4:37 AM
F/TC:0 0 probe_driver_node:436 Probing stm32-tamp on node tamp@5c00a000
D/TC:0 0 probe_driver_node:449 element: stm32-tamp on node tamp@5c00a000 deferred 2 time(s)
F/TC:0 0 probe_driver_node:436 Probing stm32-cpu-opp on node cpu0-opp-table
D/TC:0 0 probe_driver_node:449 element: stm32-cpu-opp on node cpu0-opp-table deferred 3 time(s)
D/TC:0 0 process_probe_list:590 Unresolved dependencies after 3 rounds, 3 deferred
D/TC:0 0 probe_dt_drivers_early:774 Deferred drivers probing
D/TC:0 0 print_probe_list:397 Probe list: 2 elements
D/TC:0 0 print_probe_list:399 |- Driver stm32-tamp probes on node tamp@5c00a000
D/TC:0 0 print_probe_list:399 |- Driver stm32-cpu-opp probes on node cpu0-opp-table
D/TC:0 0 print_probe_list:403 `- Probe list end
D/TC:0 0 print_probe_list:409 Failed list: 0 elements
D/TC:0 0 print_probe_list:414 `- Failed list end
Can you look in the stm32mp151.dtsi file of Optee what "@5c00a000" is for device?
Arch/arm/dts is the file located.
2024-09-12 6:40 AM
Then we have the answer!
You need to configure the special hack for USB OTG. Described inside the URL link.