2023-06-06 3:15 AM
Following the tutorial on How to customize the Linux kernel I made steps as below:
FILESEXTRAPATHS:prepend := "${THISDIR}:${THISDIR}/${PN}:"
KERNEL_CONFIG_FRAGMENTS:append = "${WORKDIR}/fragments/${LINUX_VERSION}/fragment-custom.config"
SRC_URI:append = " file://${LINUX_VERSION}/fragment-custom.config;subdir=fragments "
It seems that the kernel configuration wasn't applied at all, is there something that I'm doing wrong?
Without the FILEXTRAPATHS line, the file couldn't be found, yocto didn't look into my-layer at all.
Solved! Go to Solution.
2023-06-08 2:48 AM
Maybe you can try this instead in your layer:
KERNEL_CONFIG_FRAGMENTS:append = " \
${WORKDIR}/fragments/${LINUX_VERSION}/fragment-custom.config \
"
2023-06-06 5:00 AM
Hello @Antoni Jankowski ,
That is strange that you need this FILESEXTRAPATHS.
Did you already check if your layer was well parsed by Yocto with doing the following command ?
PC $> bitbake-layers show-layers
Kind regards,
Erwan.
2023-06-06 5:05 AM
Yes, the layer is visible and actually the first on the list of bitbake-layers show-layers. When trying without the FILESEXTRAPATHS below warning is displayed, which later turns into an error:
WARNING: /layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_5.15.bb: Unable to get checksum for linux-stm32mp SRC_URI entry fragment-custom.config: file could not be found
2023-06-06 7:34 AM
@Antoni Jankowski ,
Is it possible for you to give me a tarball containing your my-layer ? I would like to reproduce from my side to understand the issue.
Kind regards,
Erwan.
2023-06-07 1:03 AM
Sure, checkout my-layer.tar in the attachment. To replicate the issue, check the kernel config options set in my-layer/recipes-kernel/linux/linux-stm32mp/5.15/fragment-custom.config and then when the image is build and running check /proc/config.gz and compare them. In my case the options set in the fragment-custom.config are missing from the final running config.
Kind regards,
Antoni
2023-06-07 2:55 AM
Hello @Antoni Jankowski ,
Thanx for sharing, I will reproduce from my side.
Just to be sure to not face a typo issue, can you modify the name of your layer with adding "meta-" at the beginning ?
I think Yocto needs it in major situations, but I do not know in details how it can react if it does not find this prefix on a layer.
Kind regards,
erwan.
2023-06-07 3:13 AM
I think this is just the naming convention. I had to script the layer down out of all the proprietary names before sharing it with you. Anyway, I did my own fixing in the meantime, it could be so that the layer priority was at fault, as it was set to be the same as the original meta-st layers - at 6. Perhaps that through Yocto off the track. Let me know if you find something and I'll keep looking for errors as well.
2023-06-07 3:14 AM
I think this is just the naming convention. I had to script the layer down out of all the proprietary names before sharing it with you. Anyway, I did my own fixing in the meantime, it could be so that the layer priority was at fault, as it was set to be the same as the original meta-st layers - at 6. Perhaps that through Yocto off the track. Let me know if you find something and I'll keep looking for errors as well.
2023-06-07 3:21 AM
Interesting, so when you change the priority of "my-layer" to align it with the one of layer containing ST kernel, you do not have trouble anymore ?
Rgs,
Erwan.
2023-06-07 3:23 AM
I'm still waiting for the build to finish, will let you know once tested, hopefully in about an hour.