2023-02-15 05:33 AM
Hello,
Here's the context of my issue.
After the buildroot team upgraded the gcnano binaries package to v6.4.7 I'm facing flickering issues with the display. To figure out if the gcnano binaries are the root cause, I manually downgraded the gcnano to v6.4.3 in which the flickering issue is not present.
I can confirm that the same rootfs/kernel with the gcnano binaries 6.4.3 has no flickering issue.
Find attached to this post two videos :
The display is mandatory for our product and we can not accept flickering issues like this one.
How can we fix this issue ?
Let me know if you need more traces or tests.
Best Regards
Alexandre Gambier
Solved! Go to Solution.
2023-03-22 07:07 AM
I wasn't asking if you could guarantee (or ST) but only what was your personnal of view (thinking).
btw, it doesn't work.
Thanks