EMMC system upgrade from SD Card
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-05 1:32 PM
Hi,
my system working fine from EMMC(written through cube programmer). I also have on my board an SD-Card slot and boot configuration pins. Is it possible to upgrade the system through SD-Card to EMMC via dd if=... from rootfs?
How to prepare EMMC....raw file, is it possible?
I try to write sd_card.....raw file using dd application to EMMC, but the system can't start. After powering on, nothing is shown on uart debug log (boot pins changes, of course).
Thanks in advanced
BR Michal
Solved! Go to Solution.
- Labels:
-
SDIO-SDMMC
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-08 4:59 AM
I think I have a procedure, but it is complicated a little bit
Step 1. The emmc....tsv file modification
Just remove P in lines 4 and 5 and type -. Suggested create a copy of the original file because in next compilation file will be again replaced to the original content.
Step 2. Generation *.raw file
./create_sdcard_from_flashlayout.sh ../flashlayout_st-image-weston/trusted/FlashLayout_emmc_xxxx.tsv
Step 3. Copy to sd card created *.raw and tf-a-stm32mp157c...-mx-emmc.stm32 into to /usr/local for instance
Step 4. Write prepared raw image into EMMC memory by typing
dd if=/usr/local/FlashLayout_emmc_stm32mp157c-....-mx-trusted.raw of=/dev/mmcblk1 bs=8M conv=fdatasync status=progress
Step 5. Unlock the EMMC boot area
echo 0 > /sys/class/block/mmcblk1boot0/force_ro
echo 0 > /sys/class/block/mmcblk1boot1/force_ro
Step 6. Write tf-a image into the EMMC
dd if=/usr/local/tf-a-stm32mp157c-...-mx-emmc.stm32 of=/dev/mmcblk1boot0
dd if=/usr/local/tf-a-stm32mp157c-...-mx-emmc.stm32 of=/dev/mmcblk1boot1
Step 7. Mount boot partition on EMMC
mkdir -p /mnt/emmc-card
mount /dev/mmcblk1p6 /mnt/emmc-card
vi /mnt/emmc-card/extlinux.conf
Change record
root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6
to
root=/dev/mmcblk1p8
Step 8. Clean up procedure
umount /mnt/emmc-card
rm -rf /mnt/emmc-card
Step 9. Synchronize written files
sync
Step 10. Power off the board and change boot pins to EMMC
One more thing finally, to be able to store the new prepared *.raw file into /usr/local it is necessary to extend sd-card /usr/local partition. I do it like that in the file create_sdcard_from_flashlayout.sh
but this is only for the Sd-card for the EMMC go back to Your settings.
Can someone reproduce this procedure and confirm that everything is right?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-05 1:44 PM
Upgrade I mean from the previous version to the latest(4.0.2) version with partition change.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-07 6:56 AM
Hi @Michał Wołowik​ ,
eMMC contains two extra partitions (boot0 and boot1) that are not in sdcard. If these partitions are not flashed, it can explain why the system form eMMC can't start.
I would recommand to create a eMMC raw file (you may need to create a dedicated flashlayout file, and hack create_sdcard_from_flashlayout.sh script) that you put into the sdcard, and also the eMMC TF-A (ex:tf-a-stm32mp157f-ev1-emmc.stm32), then you could do something like that on your board :
dd if=<sdcard>/<eMMC image>.raw of=/dev/mmcblk1
dd if=<sdcard>/tf-a-stm32mp157f-ev1-emmc.stm32 of=/dev/mmcblk1boot0
dd if=<sdcard>/tf-a-stm32mp157f-ev1-emmc.stm32 of=/dev/mmcblk1boot1
Feel free to follow the links from the wiki to have a better understanding of these explanations.
BR,
Christophe
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-07 7:23 AM
Thanks for the answer I will try.
Yes, You have right both mmcblk1boot0 and mmcblk1boot1 are after USB programming on the EMMC memory.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-08 4:59 AM
I think I have a procedure, but it is complicated a little bit
Step 1. The emmc....tsv file modification
Just remove P in lines 4 and 5 and type -. Suggested create a copy of the original file because in next compilation file will be again replaced to the original content.
Step 2. Generation *.raw file
./create_sdcard_from_flashlayout.sh ../flashlayout_st-image-weston/trusted/FlashLayout_emmc_xxxx.tsv
Step 3. Copy to sd card created *.raw and tf-a-stm32mp157c...-mx-emmc.stm32 into to /usr/local for instance
Step 4. Write prepared raw image into EMMC memory by typing
dd if=/usr/local/FlashLayout_emmc_stm32mp157c-....-mx-trusted.raw of=/dev/mmcblk1 bs=8M conv=fdatasync status=progress
Step 5. Unlock the EMMC boot area
echo 0 > /sys/class/block/mmcblk1boot0/force_ro
echo 0 > /sys/class/block/mmcblk1boot1/force_ro
Step 6. Write tf-a image into the EMMC
dd if=/usr/local/tf-a-stm32mp157c-...-mx-emmc.stm32 of=/dev/mmcblk1boot0
dd if=/usr/local/tf-a-stm32mp157c-...-mx-emmc.stm32 of=/dev/mmcblk1boot1
Step 7. Mount boot partition on EMMC
mkdir -p /mnt/emmc-card
mount /dev/mmcblk1p6 /mnt/emmc-card
vi /mnt/emmc-card/extlinux.conf
Change record
root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6
to
root=/dev/mmcblk1p8
Step 8. Clean up procedure
umount /mnt/emmc-card
rm -rf /mnt/emmc-card
Step 9. Synchronize written files
sync
Step 10. Power off the board and change boot pins to EMMC
One more thing finally, to be able to store the new prepared *.raw file into /usr/local it is necessary to extend sd-card /usr/local partition. I do it like that in the file create_sdcard_from_flashlayout.sh
but this is only for the Sd-card for the EMMC go back to Your settings.
Can someone reproduce this procedure and confirm that everything is right?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-08 5:07 AM
One thing is strange. After programming the EMMC memory and keeping boot pins to mmc0(sd-card) during startup, the system mount rootfs not from SD-Card but EMMC. So I experimented with formatting the EMMC and then the system mount rootfs from the Sd-Card as it should. How do avoid such behaviour?
Additionally, I have a warning.
The rootfs seem to be fine.
After erasing the EMMC root, the mount point looks the same
but now it is mounted correctly
So where is the problem?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-08 5:41 AM
I think I found a solution it is necessary to change the record for mmc0 for file extlinux.conf.
Change from
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=${console},${baudrate}
to
APPEND root=/dev/mmcblk0p10 rootwait rw console=${console},${baudrate}
For me works.