cancel
Showing results for 
Search instead for 
Did you mean: 

Direct Kernel Boot on STM32MP1

HZ890
Associate

Hi everyone,

I'm attempting to optimize the boot process on my STM32MP157F-DK2 board by removing U-Boot and booting the Linux kernel directly via the FIP. I've followed the documented steps for STM32MP1:

  1. TF-A BL2 Modifications:

    • Updated STM32MP_BL33_BASE and STM32MP_BL33_MAX_SIZE in the STM32MP1 header file.

    • Increased the SDMMC timeout in stm32_sdmmc2.c to accommodate the larger kernel image.

  2. FIP Creation:

    • Recompiled TF-A with my modifications.

    • Created a new FIP where I replaced the U-Boot binary and its DTB with my Linux kernel Image and DTB.

    • The new FIP (fip.bin) now contains the kernel and DTB.

  3. Flash Layout TSV Modifications:
    I updated the TSV file to allocate a larger space for the FIP. Below is the relevant excerpt:

    HZ890_0-1742823828143.png

Despite these modifications, every time I execute the process, it fails. My questions are:

  • What is the purpose of the bootfs partition?
    Since my new FIP (fip.bin) already contains the Linux kernel and its DTB, I'm unclear why the flash layout still reserves a bootfs partition. Is it meant for additional boot configurations, an initial ramdisk, or something else?

  • Why is the u-boot-env partition still present?
    If U-Boot is being removed entirely from the boot chain, what role does the U-Boot environment play here? Is it kept for legacy or recovery purposes?

I would really appreciate any insights or suggestions on what might be going wrong or what additional changes I need to consider for a successful direct kernel boot setup on STM32MP157f-dk2.

Thanks in advance for your help!

1 REPLY 1
Erwan SZYMANSKI
ST Employee

Hello @HZ890 ,
Can you please precise a bit the status when you says "everytime I execute the process it fails" ? Do you talk at boot time or during the preparation process ? 

Do you have some error logs or anything to share ? 

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.