cancel
Showing results for 
Search instead for 
Did you mean: 

The issue of video brightness loss in H264 hardware encoder

zhutianyu
Associate

After my video data is encoded by H264 hardware, the picture becomes darker. This issue doesn't occur when displayed directly. Both the ISP and the camera preview are normal. I need some help.

board : stm32mp257f-eval

camera: imx335
hardware encoder parameters : encodebin profile="video/x-h264|element-properties,keyframe-interval=5,rate-control=0,qp-min=20,qp-max=20"

0 REPLIES 0