2024-04-27 08:43 AM
First acquaintance with STM32mp157FDK2. A couple of weeks ago I bought two sets to try. In a week I figured out how to put together my image with Yocto. And today what was supposed to happen happened. I connected the KIT to the power supply with PD3. KIT is broke. The thermal camera shows strong heating. STPMIC1APQR short circuit STPMIC1APQR. burned out. Unsuccessful test STM32mp1.
Andrew.
2024-04-27 08:58 AM - edited 2024-04-27 09:01 AM
How did you power the kit ?
Check real voltage of your power supply output.
(Your description telling nothing about, but something like this is typical for too high voltage or ESD event.)
2024-04-27 09:46 AM - edited 2024-04-27 09:56 AM
his is PD3. The voltage can be up to 20V. How do ST manage CC1 and CC2? have ST any overvoltage protection?
for ESD why didn't it work ESDA7P120-1U1M
2024-04-27 09:51 AM - edited 2024-04-27 10:02 AM
Really 20V ?
from manual UM2637 :
+
the STPMIC ds :
2024-04-27 10:00 AM - edited 2024-04-27 10:04 AM
STM32MP1157F-DK2 cannot operate power supply from PD3 source?
USB-C PD3 can provide voltage up to 20V.
2024-04-27 10:13 AM - edited 2024-04-27 10:18 AM
Hmmm- whats PD3 ?
see circuit:
CN6 is power in, 5V (3A) .
+
warning...
2024-04-27 10:17 AM
usb-c pd 3.0
2024-04-27 10:20 AM - edited 2024-04-27 10:20 AM
No. See circuit diagram... usb-c -> 5V -> to STPMIC1A .
No fast charging - only fast killing.
2024-04-27 10:23 AM - edited 2024-04-27 10:26 AM
Why isn't this written anywhere?
I threw 100€ in the trash.
2024-04-27 10:32 AM - edited 2024-04-27 10:38 AM
Come on, i just looked at the manual -> power -> and showed it here.
And if you you look at the circuit - you see the CN6 -> 5V input . Nothing else there.
So if the charger puts out 5V , everything fine. But if it tries fast charge... ok. you know now.
manual says:
btw
I have a quick charger plug , is labeled : A output : 5V , 3A ; B+C output : 5V/9V/12V , 2A .
So if using the 5V output, everything fine.