cancel
Showing results for 
Search instead for 
Did you mean: 

Is the SD Card required for the STM32MP257F-EV1

Carson
Associate III

Hello, 

 

I am working on bringing up the STM32MP257F-EV1 Development board and have a question. I was wondering if the SD card is actually required or if it and the EMMC are completely interchangeable and the whole board can work off completely off the EMMC. 

 

Thanks!

Carson

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan SZYMANSKI
ST Employee

Hello @Carson ,
The evaluation board is made to demonstrate different features, such as booting from different flash memory. So yes you can completely ignore the SD card if you want to boot from eMMC. 

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Erwan SZYMANSKI
ST Employee

Hello @Carson ,
The evaluation board is made to demonstrate different features, such as booting from different flash memory. So yes you can completely ignore the SD card if you want to boot from eMMC. 

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks Erwan!