cancel
Showing results for 
Search instead for 
Did you mean: 

Coprocessor firmware doesn't start manually via rproc

Edoardo
Associate

Hello,
I'm working on a STM32MP157D-DK1 demoboard and I want to manually start the coprocessor from u-boot.

I'm tried to follow this tutorial: MANUAL START  

The steps that I maked are:

1) I generated the code with STM32CubeMx (I selected the board STM32MP157D-DK1 with default initialization of all peripherals) 

2) I imported the code into STM32cubeIDE and I added the following changes:

In main.c:
while (1)
{
    /* USER CODE END WHILE */
    /* USER CODE BEGIN 3 */
    HAL_GPIO_TogglePin(GPIOH, GPIO_PIN_7);
    HAL_Delay(500);
}

in gpio.c:
void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = { 0 };
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  /*Configure GPIO pin*/
  GPIO_InitStruct.Pin = GPIO_PIN_7;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
}

3) I loaded the code (a simple toggle of the orange led) in production mode or Engineering mode via STM32cubeIDE and it works. 

4) I tried to starting the code from linux and it works:

02_start_from_linux.jpg

5) In the end I tried the rproc commands but without success.

I copied the file "test_mp1_CM4.elf" in the boot partition:

03_bootfs.jpg

and I tried to launch the firmware:

01_manual_boot_CM4.jpg

The led blink doesn't work.

What am I doing wrong?

 

PS: in the SDCARD I loaded the default image: en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz

Thanks.

2 REPLIES 2
Edoardo
Associate

Can anyone help me?

I attached the "elf" file.

 

mjuels
Associate II

It might be that you need to modify the linux kernel device tree to automatically attach the remoteproc probe at boot - https://wiki.st.com/stm32mpu/wiki/How_to_start_the_coprocessor_from_the_bootloader#Linux_kernel

To elaborate: If I recreate your steps with a similar "blink" elf-file, I have the same experience as you: The LED blinks when the elf is launched from linux, but not when launched from the u-boot elf.

However, when I launch the elf-from uboot, and boot into linux, I see that the remoteproc state is set to "detatched" for the m4:

 cat >/sys/class/remoteproc/remoteproc0/state
detached

 If I do not start the elf in uboot, the state is simply "offline".

When the state is detached, I can start the application using

 echo start > /sys/class/remoteproc/remoteproc0/state
 cat /sys/class/remoteproc/remoteproc0/state
running

and the blinking starts. This is consistent with the guide linked above, so maybe you need to recompile the devicetree.

Hope this helps.