2023-09-13 6:21 AM
Hello,
I'm working on a STM32MP157D-DK1 demoboard and I want to manually start the coprocessor from u-boot.
I'm tried to follow this tutorial: MANUAL START
The steps that I maked are:
1) I generated the code with STM32CubeMx (I selected the board STM32MP157D-DK1 with default initialization of all peripherals)
2) I imported the code into STM32cubeIDE and I added the following changes:
In main.c:
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_GPIO_TogglePin(GPIOH, GPIO_PIN_7);
HAL_Delay(500);
}
in gpio.c:
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = { 0 };
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
/*Configure GPIO pin*/
GPIO_InitStruct.Pin = GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
}
3) I loaded the code (a simple toggle of the orange led) in production mode or Engineering mode via STM32cubeIDE and it works.
4) I tried to starting the code from linux and it works:
5) In the end I tried the rproc commands but without success.
I copied the file "test_mp1_CM4.elf" in the boot partition:
and I tried to launch the firmware:
The led blink doesn't work.
What am I doing wrong?
PS: in the SDCARD I loaded the default image: en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Thanks.
2023-09-15 1:26 AM
2023-10-01 12:29 PM
It might be that you need to modify the linux kernel device tree to automatically attach the remoteproc probe at boot - https://wiki.st.com/stm32mpu/wiki/How_to_start_the_coprocessor_from_the_bootloader#Linux_kernel
To elaborate: If I recreate your steps with a similar "blink" elf-file, I have the same experience as you: The LED blinks when the elf is launched from linux, but not when launched from the u-boot elf.
However, when I launch the elf-from uboot, and boot into linux, I see that the remoteproc state is set to "detatched" for the m4:
cat >/sys/class/remoteproc/remoteproc0/state detached
If I do not start the elf in uboot, the state is simply "offline".
When the state is detached, I can start the application using
echo start > /sys/class/remoteproc/remoteproc0/state cat /sys/class/remoteproc/remoteproc0/state running
and the blinking starts. This is consistent with the guide linked above, so maybe you need to recompile the devicetree.
Hope this helps.