2020-02-25 09:58 AM
HI all,
I am using an STM32MP15-EV1 eval board and will connect an external amplifier to the HEADSET output. I would like this amplifier to be automatically switched on / off when sound is being played. If I am correct this is supported in the audio-graph-card machine driver via the pa-gpios property. However I cannot make this work. I am adding the following in the DT:
sound {
pa-gpios = <&gpioa 13 GPIO_ACTIVE_LOW>;
};
What else needs to be done?
Thanks,
Guillermo
2020-02-26 02:34 AM
Hi,
Which audio stack are you using ? Alsa or pulse ?
Some resources at: