2024-11-20 01:06 AM
Dear ST Team,
I'm considering purchasing a microSD card for the STM32MP157F-DK2 development board, but I want to ensure compatibility before buying.
The documentation mentions support for SanDisk Class 10 and UHS Speed Class 1 cards but doesn’t specify the maximum supported capacity. I know the board supports SDHC and SDXC standards, so theoretically, it should handle up to 2 TB (per the SDXC specification).
Here are my questions:
Any insights or experiences with high-capacity microSD cards on this board would be greatly appreciated.
Thanks in advance!
Zapsis Symeon
Solved! Go to Solution.
2024-12-17 04:12 AM - edited 2024-12-17 04:13 AM
I bought this microSD card: https://www.e-shop.gr/sandisk-sdsquac-256g-gn6ma-ultra-256gb-micro-sdxc-a1-u1-uhs-i-class-10-sd-adapter-p-PER.323711 , and it works well.
There is a small delay of about 15 minutes during the first boot (resize storage), but after that, it works perfectly.
Best regards,
Symeon
2024-12-17 04:12 AM - edited 2024-12-17 04:13 AM
I bought this microSD card: https://www.e-shop.gr/sandisk-sdsquac-256g-gn6ma-ultra-256gb-micro-sdxc-a1-u1-uhs-i-class-10-sd-adapter-p-PER.323711 , and it works well.
There is a small delay of about 15 minutes during the first boot (resize storage), but after that, it works perfectly.
Best regards,
Symeon