2024-07-21 11:09 PM
We made a new board with STM32MP157FAC1.
I tried booting with SD card with STM32MP1 Starter Package image of STM32MP157x-EV1.
I am inquiring about the following error.
NOTICE: CPU: STM32MP157FAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157F eval daughter on eval mother
INFO: PMIC version = 0x21
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
ERROR: stm32_sdmmc2_send_cmd_req: timeout 10ms (cmd = 0,status = 2000)
WARNING: CMD0, Retry: 1, Error: -60
ERROR: stm32_sdmmc2_send_cmd_req: timeout 10ms (cmd = 0,status = 2000)
WARNING: CMD0, Retry: 2, Error: -60
ERROR: stm32_sdmmc2_send_cmd_req: timeout 10ms (cmd = 0,status = 2000)
WARNING: CMD0, Retry: 3, Error: -60
ERROR: SDMMC1 init failed
PANIC at PC : 0x2ffec8ef
Exception mode=0x00000016 at: 0x2ffec8ef
Can you guess what error it is?
2024-08-02 05:34 AM
Hi @LeeJaewon ,
Except if your board is stricly same as EV1 it's normal this is not working.
You might adapt your Device Tree to you hardware.
You can refer to FAQ: STM32MP1 - How to create a device tree adapted to your design with STM32CubeMX?
Hope it help
Olivier