cancel
Showing results for 
Search instead for 
Did you mean: 

board_check_usb_power issues on EV1

BryanWang
Associate II

Hello,

After power on my EV1 board, I get the following error message:

NOTICE:  CPU: STM32MP157AAA Rev.B
NOTICE:  Model: STMicroelectronics STM32MP157C eval daughter on eval mother
NOTICE:  Board: MB1263 Var1 Rev.C-01
INFO:    Reset reason (0x15):
INFO:      Power-on Reset (rst_por)
INFO:    Using NOR
INFO:      Instance 1
INFO:    Boot used partition fsbl1
INFO:    NOR: Memory mapped mode
NOTICE:  BL2: v2.0-r1.5(debug):
NOTICE:  BL2: Built : 13:13:37, Oct  2 2018
INFO:    BL2: Doing platform setup
INFO:    PMIC version = 0x10
INFO:    RAM: DDR3-1066/888 bin G 2x4Gb 533MHz v1.45
INFO:    Memory size = 0x40000000 (1024 MB)
INFO:    BL2 runs SP_MIN setup
INFO:    BL2: Loading image id 4
INFO:    Loading image id=4 at address 0x2fff0000
INFO:    Image id=4 loaded: 0x2fff0000 - 0x30000000
INFO:    BL2: Loading image id 5
INFO:    Loading image id=5 at address 0xc0100000
INFO:    STM32 Image size : 806658
WARNING: Skip signature check (header option)
INFO:    Image id=5 loaded: 0xc0100000 - 0xc01c4f02
INFO:    read version 0 current version 0
NOTICE:  BL2: Booting BL32
INFO:    Entry point address = 0x2fff0000
INFO:    SPSR = 0x1d3
INFO:    PMIC version = 0x10
NOTICE:  SP_MIN: v2.0-r1.5(debug):
NOTICE:  SP_MIN: Built : 13:13:37, Oct  2 2018
INFO:    ARM GICv2 driver initialized
INFO:    stm32mp HSI (18): Secure only
INFO:    stm32mp HSE (20): Secure only
INFO:    stm32mp PLL2 (27): Secure only
INFO:    stm32mp PLL2_R (30): Secure only
INFO:    SP_MIN: Initializing runtime services
INFO:    SP_MIN: Preparing exit to normal world
 
 
U-Boot 2018.11-stm32mp-r3-g740edf1-dirty (Jan 03 2020 - 15:07:02 +0800)
 
CPU: STM32MP157AAA Rev.B
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
Board: stm32mp1 in trusted mode (st,stm32mp157c-dk2)
Board: MB1263 Var1 Rev.C-01
DRAM:  512 MiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
stm32 vrefbuf timed out: -110
adc@0: can't enable vdd-supply!board_check_usb_power: single shot failed for adc@0[18]!
NAND:  0 MiB
MMC:   STM32 SDMMC2: 0, STM32 SDMMC2: 1
Loading Environment from SPI Flash... Invalid bus 0 (err=-19)
*** Warning - spi_flash_probe_bus_cs() failed, using default environment
 
In:    serial
Out:   serial
Err:   serial
Net:   eth0: ethernet@5800a000
Hit any key to stop autoboot:  0 
Boot over nor0!
Saving Environment to SPI Flash... Invalid bus 0 (err=-19)
*** Warning - spi_flash_probe_bus_cs() failed, using default environment
 
Failed (-19)
Partition UBI not found!
STM32MP> 

It worked well just a few minutes ago, then this issue happened.

Could anyone help?

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
BryanWang
Associate II

oh, my fault, I took the wrong u-boot file which is for DK2 board.....

View solution in original post

1 REPLY 1
BryanWang
Associate II

oh, my fault, I took the wrong u-boot file which is for DK2 board.....