cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up the LTDC peripheral to interface with the display panel ATM0500D27-CT from AZ Displays

How to set up the LTDC peripheral to interface with the display panel ATM0500D27-CT from AZ Displays

1. Introduction


The STM32’s integrated LTDC (LCD-TFT Display Controller) peripheral can be used to interface with parallel displays. It is very common for HMI-of-Things applications to have the capability to control and display data between user and machine. 
In this article we will see how to configure the LTDC peripheral of the STM32 to interface with ATM0500D27-CT from AZ Displays – datasheet available in the link below:
https://www.azdisplays.com/PDF/ATM0500D27-CT.pdf

The display panel is available for mass market from Digi-Key:
https://www.digikey.com/en/products/detail/az-displays/ATM0500D27-CT/13236094

2. Prerequisites

  • Microcontroller: STM32F750N8
  • Software: TouchGFX Designer and STM32CubeMx

In this article we’ll see what changes need to be made to the LTDC configuration in the STM32F7508-DK TouchGFX Board Setup (TBS) to support the display panel ATM0500D27-CT.

3. Steps

 
  1. Create TouchGFX application

Create a TouchGFX application based on the STM32F7508-DK Board Setup. If you don’t know how to do this step, please refer to this link: https://support.touchgfx.com/4.18/docs/tutorials/tutorial-02
 
The tutorial uses the STM32F746G-DK while in this article we’ll be using the STM32F7508-DK.
 
  1. Open the STM32CubeMx project

Under the project location, open the STM32CubeMx project by double-clicking on STM32F7508-DK.ioc
 
 
 

613.png

  1. Set up the LTDC clock

When we look at the display panel datasheet, we see the specification of the pixel clock or dot clock “DCLK”. This pixel clock is the speed at which pixels are transmitted. It is specified in MHz and for this panel it is 25MHz typ.
 
 
 614.png

 
In STM32CubeMx, under the Clock Configuration Tab, is where the pixel clock is set up. As shown below, the LCD-TFT clock is derived from PLLSAI1. Thus, we need to set up the PLLSAI1 “N” multiplier, “R” and the divider right after the output of the PLLSAI1  in a way to get 25MHz to the LCD-TFT. 

One possible solution is to have N = 100, R = 2, and the divider right after the output of the PLLSAI1 = 2 . This solution gives a pixel clock of 25MHz.
616.png
  1. Set up the display type

When we look at the general specifications of the display panel, we see the display interface supports 24-bit RGB:
617.png
Under Pinout & Configuration Tab, we select Multimedia category and then LTDC peripheral. Under LTDC Mode and Configuration, we select the display Type: RGB888 (24 bits).

 
 
 618.png
 
​​​​​​
  1. Setup the horizontal and vertical timings

The Timing Table of the display panel shows the horizontal and vertical timings:
  1. The horizontal timings highlighted below gives a display period of 800 which is the same as display width. Besides, it gives a back porch of 8, a front porch 8, and a pulse width or horizontal synchronization width of 4.
 
 620.png

 
Under Parameter Settings, we provision the horizontal timings given by the datasheet of the display panel as shown below:
 
 621.png
 
  1. The same timing table in the datasheet of the display gives the vertical timings: display period of 480 which is the same Active height. Besides, it gives a back porch of 8, a front porch 8, and a pulse width or vertical synchronization width of 4.
 
 623.png

 
Under Parameter Settings and then Synchronization for Height, we provision the vertical timings given by the datasheet of the display panel as shown below:
 
 
 624.png

 
  1. Signal Polarity

The display panel supports three modes: SYNC mode, SYNC-DE mode, and DE mode. We’re more interested in SYNC-DE mode as it uses the three signals: Pixel clock (DCLK), HSYNC, VSYNC, and Data Enable (DE).
625.png
The display panel has already VDPOL and HDPOL tied to High. This means the VSYNC and HSYNC are active low. Besides, the figure below shows the DE signal is active high.
 
 626.png

       
Based on the signal polarity given by the datasheet of the display panel, we provision the configuration under Signal Polarity.
 
 627.png
  1. Set up the layer settings

We will match the layer settings to the display settings:
  • Horizontal Stop to the display width which is 800
  • Vertical stop to the display height which is 480
  • Pixel format to the display type which is RGB888
  • Frame buffer Line Length to the display width which is 800
  • Frame buffer number of lines to the display width which is 480
 
 628.png

 

4. Links

STM32F7508N8 – Datasheet
STM32F75xxx and STM32F74xxx advanced arm based 32-bit MCUs- Reference manual
STM32CubeMx - STM32Cube initialization code generator
STM32F7508-DK - Discovery kit with STM32F750N8 MCU
AN4861: LCD-TFT display controller (LTDC) on STM32 MCUs - Application Note

 
 
 
Comments
Cfarq.1
Associate

Hi Laura,

I was using your guide to setup an AZ display. However, I am not able to change the color within the hltdc.Init.Backcolor to ensure proper functionality, it remains all white. I want to make sure I do not have something configured wrong and determine if it's hardware related. Can you please let me know if a setting seems off to you?

I’m using a custom board with a STM32F479BIT6 (PH0/PH1 8Mhz oscillator only) interfacing with a ATM0500D27K.

RCC config:
_legacyfs_online_stmicro_images_0693W00000JOJFiQAP.pngSYS Config:


_legacyfs_online_stmicro_images_0693W00000JOIrsQAH.pngLTDC Config:


_legacyfs_online_stmicro_images_0693W00000JOJIwQAP.png
_legacyfs_online_stmicro_images_0693W00000JOJJuQAP.png 


_legacyfs_online_stmicro_images_0693W00000JOJKJQA5.png
_legacyfs_online_stmicro_images_0693W00000JOJK4QAP.png
_legacyfs_online_stmicro_images_0693W00000JOJLCQA5.png
_legacyfs_online_stmicro_images_0693W00000JOJLRQA5.pngClock Config:


_legacyfs_online_stmicro_images_0693W00000JOJM0QAP.pngLTDC GPIO config:


_legacyfs_online_stmicro_images_0693W00000JOJMFQA5.png

SPoor.1
Associate

Hi @Laura C.​ , thanks a lot for your post. Just a small note:

"Only the DE control signal must be inverted versus the DE polarity indicated in the display

datasheet. The other control signals must be configured exactly like the display datasheet."

ZExpo.1
Senior

Hi,

I have setup the STM32F7508-DK according to the article published by ST, I am using 7" 800x480 TFT with the STM32F7508-DK Board, The Problem lies when the Image is updated for there is the transition of Screens, I.e The Screen Updates randomly in a blocked fashion, I am unable to find the issue, I would appreciate if you could provide some lead on the same.

Version history
Last update:
‎2021-12-03 8:35 AM