How to create an STM32N6 FSBL load and run
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Email to a Friend
- Printer Friendly Page
- Report Inappropriate Content
on
‎2025-02-14
4:48 AM
- edited on
‎2025-02-20
6:23 AM
by
Laurids_PETERSE
Summary
The first stage bootloader (FSBL) is a key component in the boot process of STM32N6 microcontrollers. It is responsible for initializing the system, configuring the hardware, and loading the application code from external memory into the internal or external memories for execution. This article provides a quick tutorial on how to use the FSBL in the load and run mode including the process to program the external memory.
It covers two practical examples, the first being a simple blink LED application running directly from the FSBL. The second being a more useful setup, where the FSBL loads an application from external memory and runs it from the internal RAM.
Introduction
At power-on, the boot ROM copies the FSBL binary from the external memory into the internal SRAM. Once the boot ROM task is completed, it will jump to the FSBL project, which is usually responsible for executing the clock and system settings, and configuring the external memories. Finally, it either copies the application binary in internal SRAM or sets the external memory in memory mode. When done, the application itself starts up and runs. If you want to know more about the boot ROM, check this knowledge article.
On STM32N6 MCUs, the first-stage bootloader (FSBL) must be signed or at least have a valid header, so the boot ROM can execute it in a secured-locked state. The FSBL layout includes several key components, and more details are available in this article.
This article uses the STM32N6570-DK as the base for its hands-on portion, but the content can be tailored to any specific STM32N6 hardware. Two examples are shown: the first example is a simple blink LED running directly from the FSBL, and the second example is composed of two binaries, the application and FSBL. Both examples have the header added and programmed on the external memory. It is up to the FSBL to execute the application directly from the internal RAM, or copy from the external FLASH to the internal RAM and execute the application.
1. FSBL main features
The FSBL can be used in several different ways, each suited to specific application requirements. The following sections describe the two modes that the FSBL is used in this article.
1.1 Application as part of the FSBL
In this mode, the boot ROM fetches the FSBL from external serial NOR flash memory. As the FSBL and application are contained in the same binary, there is a 511 KB size limitation in this mode. This is due to the total area of 512 KB that the boot ROM copies from the external memory into the internal SRAM. The visual representation can be observed in the small animation below:
1.2 FSBL with load & run application
In this mode, the boot ROM fetches the FSBL from external flash memory. This time, the FSBL proceeds to configure the external memory and fetch a second binary stored in it, then copy it into the internal SRAM. Once the binary is loaded, the FSBL jumps to the new position in RAM, where the application code is located and starts the execution. This mode is applicable to a few examples available in the STM32Cube_FW_N6. The interesting aspect is that the 511 KB size limitation is no longer applicable, as the user code can be placed in the remaining area of the internal RAM.
2. Hands-on with blink LED
This article assumes you have installed STM32CubeMX (6.13 or later), the latest version of the STM32N6 HAL driver, STM32CubeProgrammer (2.18 or later), and STM32CubeIDE (1.17.0 or later). The hardware used to showcase is the STM32N6570-DK and make sure you have it in DEV boot mode to program the code:
2.1 First demo with simple FSBL blink code
The project needs to configure a few peripherals to properly work, including the green LED associated with the PO1 and its active HIGH to validate the first step. Also, the FSBL and application being in the same binary. So, let us start with this initial configuration first.
Create a new project using the STM32CubeMX and select the [STM32N657X0H3Q]. Select the option to use the [Secure Domain only].
2.1.1 Configure the LED pin
Locate the PO1 and configure it as GPIO_Output and use the label to name it GREEN_LED.
We need to assign the GPIO to be used by the FSBL
2.1.2 Code generation and editing
In the [Project Manager] tab, ensure the [FSBL] checkbox is selected and generate the code for your preferred toolchain.
Once the project is created, add these two lines in the main loop:
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_GPIO_TogglePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin);
HAL_Delay(100);
}
/* USER CODE END 3 */
Make sure that your project settings are configured to generate the *.bin as well, since we use it to run the scripts.
Enter in debug mode and validate that your code is working. Now that you have, we need to add the FSBL header to ensure that the boot ROM is capable of reading and copying it from the external memory. To do this, we use the STM32CubeProgrammer’s CLI. The next assumes the STM32CubeProgrammer was installed in the default path, if not, make sure to adjust it accordingly.
2.1.3 Adding the header
To facilitate the process, its possible to type [cmd] in the binary folder. For example ..\LED_Toggle\STM32CubeIDE\FSBL\Debug. This will pop up the cmd in the selected path and its possible to use the command below:
"C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_SigningTool_CLI.exe" -bin LED_Toggle_FSBL.bin -nk -of 0x80000000 -t fsbl -o Project-trusted.bin -hv 2.3 -dump Project-trusted.bin
This creates the header for the binary, which can now be loaded into the external FLASH using STM32CubeProgrammer.
2.1.4 Programming the binary
Make sure that the external loader for the flash memory is enabled and use the address [0x7000 0000] to program the binary.
TIP: you might need to power cycle the board in case a failure message appears when clicking [Start Programming].
To validate the entire process worked, disconnect from the STM32CubeProgrammer. Then switch BOOT1 to 0 and reset the board. This ensures that the boot ROM uses the external memory and the green LED should blink.
2.2 Second demo with FSBL and application
Now that we concluded the process to run our simple code from the FSBL, it's time to implement the second example. This example consists of having the FSBL to copy the application content from the external FLASH to internal RAM, and executing the code from there.
2.2.1 Configure the XSPI and XSPIM
Using the same STM32CubeMX project, locate the [XSPIM] under the [Connectivity] menu on the left and select it to run during the [FSBL] and have the [Direct] mode selected:
The OCTOSPI flash memory has the following characteristics: 1 Gbit, 1.8 V, 200 MHz, DTR, read while writing. It is connected to the OCTOSPI interface of the STM32N657X0H3Q microcontroller on the STM32N6570-DK board on XSPI2. With that information, go to XSPI2 to configure the peripheral according to the hardware available:
As for the [Parameter Settings], look carefully at the image below:
2.2.2 Configure the EXTMEM_MANAGER
The next step is locating the [Middleware and Software Packs] in the [Categories]. Expand the [EXTMEM_MANAGER]. Add the FSBL and activate it using the following settings:
[LRUN source address offset] = 0x00100000
[LRUN source code size] = 0x10000
[LRUN destination address] = 0x34000000
In the [Memory 1] tab, ensure its as follows:
2.2.3 Configure the XSPI clock
The last step for the XSPI is to configure its clock. For this example, we will set the XPI2 clock to 50 MHz. To achieve higher speeds up to the 200 MHz supported by this serial NOR FLASH, you need to make changes to OTP for I/O speed optimization, which is not covered in this article. Go to the [Clock Configuration] tab and have the IC3 as the source for the XSPI2 and type 50 and press enter for the clock to be automatically adjusted:
2.2.4 Code generation and build
Now that we are done with the XSPI, it is time to add the [APPLI] checkbox in the [Project Manager] tab, so the application project can be created:
And roll back to the [Pinout & Configuration] tab to change the [GPIO] LED pin to be assigned to the application instead of the FSBL:
Proceed with the code generation for both projects.
In the _Appli project, locate the main.c file and add the toggle LED function call in its main loop:
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_GPIO_TogglePin(GREEN_LED_GPIO_Port, GREEN_LED_Pin);
HAL_Delay(200);
}
/* USER CODE END 3 */
In the FSBL project, remove the previous user code portion in the main.c file, responsible for the LED toggling we had in the first hands-on. Make sure to either change the #define EXTMEM_HEADER_OFFSET from 0x0 to 0x400 in the stm32_boot_lrun.c or define it in the stm32_boot_lrun.h. The reason is that our application also has the 1 KB header, added by the script.
2.2.5 Adding the header and programming the binaries
Build both projects, making sure the *.bin is created for both the _Appli and the _FSBL projects. Once the build is done successfully, we perform the same step of calling the STM32CubeProgarmmer’s CLI in each of the binaries respective folder to perform the signing. These are the commands:
FSBL:
"C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_SigningTool_CLI.exe" -bin LED_Toggle_FSBL.bin -nk -of 0x80000000 -t fsbl -o FSBL-trusted.bin -hv 2.3 -dump FSBL-trusted.bin
Application:
"C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_SigningTool_CLI.exe" -bin LED_Toggle_Appli.bin -nk -of 0x80000000 -t fsbl -o Appli-trusted.bin -hv 2.3 -dump Appli-trusted.bin
Use the same process using the STM32CubeProgrammer to program the FSBL at address 0x7000 0000 and the appli at address 0x7010 0000. Remember to have the STM32N6’s BOOT1 set to HIGH and reset or power cycle the board before programming.
2.2.6 Validation
To see your application running, have the BOOT1 set to LOW, disconnect the programmer and power cycle. Now, you have the green LED blinking with the code copied from the external flash into the internal RAM by your custom FSBL!
Conclusion
By understanding the FSBL layout and its main features, developers can effectively utilize the FSBL to meet their specific needs. This article has provided a hands-on tutorial using the STM32N6570 discovery kit. demonstrating how to implement and run applications directly from the FSBL and how to configure the FSBL to load and run applications from external memory. By following these steps, developers can ensure a smooth and efficient boot process for their STM32N6-based projects.
Related links
- User manual 3234: How to proceed with boot ROM on STM32N6 MCUs
- User manual 3249: Getting started with STM32CubeN6 for STM32N6 series
- User manual 3300: Discovery kit with STM32N657X0 MCU
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi @B.Montanari ! Thanks a lot for this informative tutorial! Would you mind attaching the resulting project to the article, and also the known-to-work binaries (FSBL and Appli, ideally both signed and without header)?
I followed your guide but the Appli binary seems to not boot, and having these files would help me (and probably others as well) debug the issue.
Thanks, Michael
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi @asdfasdf ,
Thanks for the feedback!
I've uploaded the entire source code for this particular article in our STM32 HotSpot github page> stm32-hotspot/STM32N6_FSBL_Modes , hope it helps.
We also have the templates in the HAL driver repo, assuming the default installation folder, the template should be here> C:\Users\%username%\STM32Cube\Repository\STM32Cube_FW_N6_V1.0.0\Projects\STM32N6570-DK\Templates\Template_FSBL_LRUN
Let me know if you have any follow up questions.
Best Regards
Bruno
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
I had the same problem as the OP where the Appli binary wouldn't boot. Upon comparing the code shared by Bruno on Github I noticed the clock for IC3 in XSPI2 was set to 32MHz instead of 50MHz as per this guide. Once I set it to 32MHz and re-built, the Apply binary successfully booted. This change looks to have also made the clock solver to adjust other clocks as well, albeit to different values than what is in the Github repo.
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
@flexiglass In my case the problem wasn't the XSPI2 clock (that works for me at 50 MHz as in the tutorial), but the SYSB clock (which feeds the AXI). I had this running at 400 MHz whereas @B.Montanari uses just 64 MHz. Lowering SYSB to 64 MHz made it work for me, and it also continues to work even if I increase the CPU clock (SYSA) to 600 MHz.
I have no idea why it is so sensitive to the SYSB clock, as that should not really have to do anything with the external flash I guess? I have the exact same problem when doing XIP instead of LRUN and asked about it here, sadly without an answer so far. This is pretty disappointing, as the MCU is dead-slow with RAM running at just 64 MHz...
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi @flexiglass and @asdfasdf ,
I've just made some changes in the *.ioc file to run the CPU at 600MHz, AXISRAM at 400MHz and kept the IC3 (XSPI2) at 50MHz. Please see the attached *.ioc. In this version I've also added the ICACHE and DCACHE plus the MPU settings, so we should have the fastest performance results without going into overdrive mode, which allows the core to go up to 800MHz. The zip for the changed project is here> STM32N6_FSBL_Modes/LoadAndRun/LoadAndRun_600MHz.7z at main · stm32-hotspot/STM32N6_FSBL_Modes
I'm planning on writing a quick article on the overdrive and another one on the OTP programming, so I could detail more on how to change the settings to get a higher clock on the XSPI2 in a reliable manner as well. I'll have a code example for that as well once I'm done.
Hope this helps and don't forget to change the #define EXTMEM_HEADER_OFFSET to 0x400 after code generation.
The final comment, if you want to avoid always using the CLI, you can have it as a post build command:. Go to the project properties, C/C++ Build, Settings then type this command in the Build Steps tab under the Post-build steps:
cd "${ProjDirPath}/Debug" && echo y | "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_SigningTool_CLI.exe" -bin "${ProjName}.bin" -nk -of 0x80000000 -t fsbl -o "${ProjName}-Trusted.bin" -hv 2.3 -dump "${ProjName}-Trusted.bin"
You can use the same command for the Appli and FSBL projects.
Best Regards
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi @B.Montanari , thank you very much for your help in resolving this issue! Sadly, even flashing the compiled binaries that you uploaded the board does not start (that is, no blinking LED). I'm starting to suspect something might be wrong with my Discovery board, or that this is due to differing OTP fuse configurations. I have not changed anything in this regard but am using the Discovery board exactly in the state I bought it.
I have attached an Export of the OTP settings generated by CubeProg - would you mind doing the same for your board (where this is apparently working) and diffing with mine to see whether there are any differences?
Also, I attached three photos showing the exact hardware revision of the Discovery board and MCU - it would be great if you could check this against your version as well, just to make sure I'm not having a broken hardware revision or something like that.
Thank you very much!
Best regards, Michael
Name | Word | Value | Status | Lock
---------------------------------------------------+-----------------+-----------------+-----------------+----------------
OTP_HW_WORD0 | OTP0 | 0xAAAA5555 | 0x40000000 | Yes
OTP_HW_WORD1 | OTP1 | 0x0000000F | 0x00000000 | No
OTP_HW_WORD2 | OTP2 | 0x00000000 | 0x00000000 | No
OTP_HW_WORD3 | OTP3 | 0x00000000 | 0x00000000 | No
OTP_HW_WORD4 | OTP4 | 0x0000F0FF | 0x00000000 | No
ID0 | OTP5 | 0x0044002E | 0x40000000 | Yes
ID1 | OTP6 | 0x4236500E | 0x40000000 | Yes
ID2 | OTP7 | 0x0036324E | 0x40000000 | Yes
OTP_RPN_OPTION | OTP8 | 0xFFFFFFFF | 0x40000000 | Yes
OTP_RPN_CODING | OTP9 | 0x00002000 | 0x40000000 | Yes
BOOTROM_CONFIG_1 | OTP10 | 0x00030103 | 0x00000000 | No
BOOTROM_CONFIG_2 | OTP11 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_3 | OTP12 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_4 | OTP13 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_5 | OTP14 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_6 | OTP15 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_7 | OTP16 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_8 | OTP17 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_9 | OTP18 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_10 | OTP19 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_11 | OTP20 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_12 | OTP21 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_13 | OTP22 | 0x00000000 | 0x00000000 | No
BOOTROM_CONFIG_14 | OTP23 | 0x36FC814F | 0x40000000 | Yes
BOOT_TZ_EPOCH0 | OTP24 | 0x00000000 | 0x00000000 | No
BOOT_TZ_EPOCH1 | OTP25 | 0x00000000 | 0x00000000 | No
BOOT_TZ_EPOCH2 | OTP26 | 0x00000000 | 0x00000000 | No
BOOT_TZ_EPOCH3 | OTP27 | 0x00000000 | 0x00000000 | No
BOOT_TZ_EPOCH4 | OTP28 | 0x00000000 | 0x00000000 | No
BOOT_TZ_EPOCH5 | OTP29 | 0x00000000 | 0x00000000 | No
BOOT_TZ_EPOCH6 | OTP30 | 0x00000000 | 0x00000000 | No
BOOT_TZ_EPOCH7 | OTP31 | 0x00000000 | 0x00000000 | No
BOOT_NS_EPOCH0 | OTP32 | 0x00000000 | 0x00000000 | No
BOOT_NS_EPOCH1 | OTP33 | 0x00000000 | 0x00000000 | No
BOOT_NS_EPOCH2 | OTP34 | 0x00000000 | 0x00000000 | No
BOOT_NS_EPOCH3 | OTP35 | 0x00000000 | 0x00000000 | No
BOOT_NS_EPOCH4 | OTP36 | 0x00000000 | 0x00000000 | No
BOOT_NS_EPOCH5 | OTP37 | 0x00000000 | 0x00000000 | No
BOOT_NS_EPOCH6 | OTP38 | 0x00000000 | 0x00000000 | No
BOOT_NS_EPOCH7 | OTP39 | 0x00000000 | 0x00000000 | No
available to customer | OTP40 | 0x00000000 | 0x00000000 | No
available to customer | OTP41 | 0x00000000 | 0x00000000 | No
available to customer | OTP42 | 0x00000000 | 0x00000000 | No
available to customer | OTP43 | 0x00000000 | 0x00000000 | No
available to customer | OTP44 | 0x00000000 | 0x00000000 | No
available to customer | OTP45 | 0x00000000 | 0x00000000 | No
available to customer | OTP46 | 0x00000000 | 0x00000000 | No
available to customer | OTP47 | 0x00000000 | 0x00000000 | No
available to customer | OTP48 | 0x00000000 | 0x00000000 | No
available to customer | OTP49 | 0x00000000 | 0x00000000 | No
available to customer | OTP50 | 0x00000000 | 0x00000000 | No
available to customer | OTP51 | 0x00000000 | 0x00000000 | No
available to customer | OTP52 | 0x00000000 | 0x00000000 | No
available to customer | OTP53 | 0x00000000 | 0x00000000 | No
available to customer | OTP54 | 0x00000000 | 0x00000000 | No
available to customer | OTP55 | 0x00000000 | 0x00000000 | No
TAMP_EN | OTP56 | 0x00000000 | 0x00000000 | No
TAMP_CFM | OTP57 | 0x00000000 | 0x00000000 | No
TAMP_CFG | OTP58 | 0x00000000 | 0x00000000 | No
available to customer | OTP59 | 0x00000000 | 0x00000000 | No
available to customer | OTP60 | 0x00000000 | 0x00000000 | No
available to customer | OTP61 | 0x00000000 | 0x00000000 | No
available to customer | OTP62 | 0x00000000 | 0x00000000 | No
available to customer | OTP63 | 0x00000000 | 0x00000000 | No
available to customer | OTP64 | 0x00000000 | 0x00000000 | No
available to customer | OTP65 | 0x00000000 | 0x00000000 | No
available to customer | OTP66 | 0x00000000 | 0x00000000 | No
available to customer | OTP67 | 0x00000000 | 0x00000000 | No
available to customer | OTP68 | 0x00000000 | 0x00000000 | No
available to customer | OTP69 | 0x00000000 | 0x00000000 | No
available to customer | OTP70 | 0x00000000 | 0x00000000 | No
available to customer | OTP71 | 0x00000000 | 0x00000000 | No
available to customer | OTP72 | 0x00000000 | 0x00000000 | No
available to customer | OTP73 | 0x00000000 | 0x00000000 | No
available to customer | OTP74 | 0x00000000 | 0x00000000 | No
available to customer | OTP75 | 0x00000000 | 0x00000000 | No
available to customer | OTP76 | 0x00000000 | 0x00000000 | No
available to customer | OTP77 | 0x00000000 | 0x00000000 | No
available to customer | OTP78 | 0x00000000 | 0x00000000 | No
available to customer | OTP79 | 0x00000000 | 0x00000000 | No
available to customer | OTP80 | 0x00000000 | 0x00000000 | No
available to customer | OTP81 | 0x00000000 | 0x00000000 | No
available to customer | OTP82 | 0x00000000 | 0x00000000 | No
available to customer | OTP83 | 0x00000000 | 0x00000000 | No
available to customer | OTP84 | 0x00000000 | 0x00000000 | No
available to customer | OTP85 | 0x00000000 | 0x00000000 | No
available to customer | OTP86 | 0x00000000 | 0x00000000 | No
available to customer | OTP87 | 0x00000000 | 0x00000000 | No
available to customer | OTP88 | 0x00000000 | 0x00000000 | No
available to customer | OTP89 | 0x00000000 | 0x00000000 | No
available to customer | OTP90 | 0x00000000 | 0x00000000 | No
available to customer | OTP91 | 0x00000000 | 0x00000000 | No
available to customer | OTP92 | 0x00000000 | 0x00000000 | No
available to customer | OTP93 | 0x00000000 | 0x00000000 | No
available to customer | OTP94 | 0x00000000 | 0x00000000 | No
available to customer | OTP95 | 0x00000000 | 0x00000000 | No
Reserved | OTP96 | 0x1F38978A | 0x40000000 | Yes
Reserved | OTP97 | 0x00251132 | 0x40000000 | Yes
Reserved | OTP98 | 0x00000130 | 0x40000000 | Yes
Reserved | OTP99 | 0x00007889 | 0x40000000 | Yes
Reserved | OTP100 | 0x00000000 | 0x00000000 | No
Reserved | OTP101 | 0x00000000 | 0x00000000 | No
Reserved | OTP102 | 0x00000000 | 0x00000000 | No
Reserved | OTP103 | 0xC57E7E55 | 0x40000000 | Yes
Reserved | OTP104 | 0x00000000 | 0x40000000 | Yes
Reserved | OTP105 | 0x00000000 | 0x40000000 | Yes
Reserved | OTP106 | 0x46523E53 | 0x40000000 | Yes
Reserved | OTP107 | 0x00000000 | 0x00000000 | No
Reserved | OTP108 | 0x00000000 | 0x00000000 | No
Reserved | OTP109 | 0x00000000 | 0x00000000 | No
Reserved | OTP110 | 0x00000718 | 0x40000000 | Yes
Reserved | OTP111 | 0x00000000 | 0x40000000 | Yes
Reserved | OTP112 | 0x00000000 | 0x00000000 | No
Reserved | OTP113 | 0x00763331 | 0x40000000 | Yes
Reserved | OTP114 | 0x80000249 | 0x00000000 | No
Reserved | OTP115 | 0x00000000 | 0x40000000 | Yes
Reserved | OTP116 | 0x00000000 | 0x00000000 | No
Reserved | OTP117 | 0x00000000 | 0x00000000 | No
Reserved | OTP118 | 0x00000000 | 0x00000000 | No
Reserved | OTP119 | 0x00000000 | 0x00000000 | No
Reserved | OTP120 | 0x3047C60E | 0x40000000 | Yes
Reserved | OTP121 | 0x013B8079 | 0x40000000 | Yes
Reserved | OTP122 | 0x93C0078C | 0x40000000 | Yes
Reserved | OTP123 | 0x9E087777 | 0x40000000 | Yes
HCONF1 | OTP124 | 0x00018000 | 0x00000000 | No
Reserved | OTP125 | 0x00000000 | 0x40000000 | Yes
Reserved | OTP126 | 0x00000000 | 0x40000000 | Yes
Reserved | OTP127 | 0x00000000 | 0x40000000 | Yes
STM32_CERTIF0 | OTP128 | 0xC0EF8743 | 0x40000000 | Yes
STM32_CERTIF1 | OTP129 | 0x56A778B1 | 0x40000000 | Yes
STM32_CERTIF2 | OTP130 | 0xF080A19E | 0x40000000 | Yes
STM32_CERTIF3 | OTP131 | 0xF8FA0E42 | 0x40000000 | Yes
STM32_CERTIF4 | OTP132 | 0xC7DD2450 | 0x40000000 | Yes
STM32_CERTIF5 | OTP133 | 0x6E0B01B1 | 0x40000000 | Yes
STM32_CERTIF6 | OTP134 | 0x0B1FC481 | 0x40000000 | Yes
STM32_CERTIF7 | OTP135 | 0x3D40305F | 0x40000000 | Yes
STM32_CERTIF8 | OTP136 | 0x9A7662EE | 0x40000000 | Yes
STM32_CERTIF9 | OTP137 | 0x7EA6323A | 0x40000000 | Yes
STM32_CERTIF10 | OTP138 | 0x05BF7294 | 0x40000000 | Yes
STM32_CERTIF11 | OTP139 | 0xF85E01B4 | 0x40000000 | Yes
STM32_CERTIF12 | OTP140 | 0x105B9B8A | 0x40000000 | Yes
STM32_CERTIF13 | OTP141 | 0x30769158 | 0x40000000 | Yes
STM32_CERTIF14 | OTP142 | 0xF4EEBD72 | 0x40000000 | Yes
STM32_CERTIF15 | OTP143 | 0x71DE1D05 | 0x40000000 | Yes
STM32PUBKEY0 | OTP144 | 0x151AA162 | 0x40000000 | Yes
STM32PUBKEY1 | OTP145 | 0x1FC421F5 | 0x40000000 | Yes
STM32PUBKEY2 | OTP146 | 0xC099CF18 | 0x40000000 | Yes
STM32PUBKEY3 | OTP147 | 0x5017C2A9 | 0x40000000 | Yes
STM32PUBKEY4 | OTP148 | 0xEE5462AE | 0x40000000 | Yes
STM32PUBKEY5 | OTP149 | 0x7E691775 | 0x40000000 | Yes
STM32PUBKEY6 | OTP150 | 0xCC771020 | 0x40000000 | Yes
STM32PUBKEY7 | OTP151 | 0x275B9E70 | 0x40000000 | Yes
STM32PUBKEY8 | OTP152 | 0x4CE648A4 | 0x40000000 | Yes
STM32PUBKEY9 | OTP153 | 0x8BF2D84C | 0x40000000 | Yes
STM32PUBKEY10 | OTP154 | 0xCEF0E429 | 0x40000000 | Yes
STM32PUBKEY11 | OTP155 | 0x855984EB | 0x40000000 | Yes
STM32PUBKEY12 | OTP156 | 0x1A63E8DC | 0x40000000 | Yes
STM32PUBKEY13 | OTP157 | 0x47B71FAE | 0x40000000 | Yes
STM32PUBKEY14 | OTP158 | 0x4644432D | 0x40000000 | Yes
STM32PUBKEY15 | OTP159 | 0x5B0B721A | 0x40000000 | Yes
OTP_ROT_HASH0 | OTP160 | 0x00000000 | 0x00000000 | No
OTP_ROT_HASH1 | OTP161 | 0x00000000 | 0x00000000 | No
OTP_ROT_HASH2 | OTP162 | 0x00000000 | 0x00000000 | No
OTP_ROT_HASH3 | OTP163 | 0x00000000 | 0x00000000 | No
OTP_ROT_HASH4 | OTP164 | 0x00000000 | 0x00000000 | No
OTP_ROT_HASH5 | OTP165 | 0x00000000 | 0x00000000 | No
OTP_ROT_HASH6 | OTP166 | 0x00000000 | 0x00000000 | No
OTP_ROT_HASH7 | OTP167 | 0x00000000 | 0x00000000 | No
ST_RSSE_EDMK_DERIV_CSTE_FUSE | OTP168 | 0x4FB6E1A0 | 0x40000000 | Yes
OTP_MAC1_ADDR_LOW | OTP169 | 0x00000000 | 0x00000000 | No
OTP_MAC1_ADDR_HIGH | OTP170 | 0x00000000 | 0x00000000 | No
OTP_MAC2_ADDR_LOW | OTP171 | 0x00000000 | 0x00000000 | No
OTP_MAC2_ADDR_HIGH | OTP172 | 0x00000000 | 0x00000000 | No
available to customer | OTP173 | 0x00000000 | 0x00000000 | No
available to customer | OTP174 | 0x00000000 | 0x00000000 | No
available to customer | OTP175 | 0x00000000 | 0x00000000 | No
available to customer | OTP176 | 0x00000000 | 0x00000000 | No
available to customer | OTP177 | 0x00000000 | 0x00000000 | No
available to customer | OTP178 | 0x00000000 | 0x00000000 | No
available to customer | OTP179 | 0x00000000 | 0x00000000 | No
available to customer | OTP180 | 0x00000000 | 0x00000000 | No
available to customer | OTP181 | 0x00000000 | 0x00000000 | No
available to customer | OTP182 | 0x00000000 | 0x00000000 | No
available to customer | OTP183 | 0x00000000 | 0x00000000 | No
available to customer | OTP184 | 0x00000000 | 0x00000000 | No
available to customer | OTP185 | 0x00000000 | 0x00000000 | No
available to customer | OTP186 | 0x00000000 | 0x00000000 | No
available to customer | OTP187 | 0x00000000 | 0x00000000 | No
available to customer | OTP188 | 0x00000000 | 0x00000000 | No
available to customer | OTP189 | 0x00000000 | 0x00000000 | No
available to customer | OTP190 | 0x00000000 | 0x00000000 | No
available to customer | OTP191 | 0x00000000 | 0x00000000 | No
available to customer | OTP192 | 0x00000000 | 0x00000000 | No
available to customer | OTP193 | 0x00000000 | 0x00000000 | No
available to customer | OTP194 | 0x00000000 | 0x00000000 | No
available to customer | OTP195 | 0x00000000 | 0x00000000 | No
available to customer | OTP196 | 0x00000000 | 0x00000000 | No
available to customer | OTP197 | 0x00000000 | 0x00000000 | No
available to customer | OTP198 | 0x00000000 | 0x00000000 | No
available to customer | OTP199 | 0x00000000 | 0x00000000 | No
available to customer | OTP200 | 0x00000000 | 0x00000000 | No
available to customer | OTP201 | 0x00000000 | 0x00000000 | No
available to customer | OTP202 | 0x00000000 | 0x00000000 | No
available to customer | OTP203 | 0x00000000 | 0x00000000 | No
available to customer | OTP204 | 0x00000000 | 0x00000000 | No
available to customer | OTP205 | 0x00000000 | 0x00000000 | No
available to customer | OTP206 | 0x00000000 | 0x00000000 | No
available to customer | OTP207 | 0x00000000 | 0x00000000 | No
available to customer | OTP208 | 0x00000000 | 0x00000000 | No
available to customer | OTP209 | 0x00000000 | 0x00000000 | No
available to customer | OTP210 | 0x00000000 | 0x00000000 | No
available to customer | OTP211 | 0x00000000 | 0x00000000 | No
available to customer | OTP212 | 0x00000000 | 0x00000000 | No
available to customer | OTP213 | 0x00000000 | 0x00000000 | No
available to customer | OTP214 | 0x00000000 | 0x00000000 | No
available to customer | OTP215 | 0x00000000 | 0x00000000 | No
available to customer | OTP216 | 0x00000000 | 0x00000000 | No
available to customer | OTP217 | 0x00000000 | 0x00000000 | No
available to customer | OTP218 | 0x00000000 | 0x00000000 | No
available to customer | OTP219 | 0x00000000 | 0x00000000 | No
available to customer | OTP220 | 0x00000000 | 0x00000000 | No
available to customer | OTP221 | 0x00000000 | 0x00000000 | No
available to customer | OTP222 | 0x00000000 | 0x00000000 | No
available to customer | OTP223 | 0x00000000 | 0x00000000 | No
available to customer | OTP224 | 0x00000000 | 0x00000000 | No
available to customer | OTP225 | 0x00000000 | 0x00000000 | No
available to customer | OTP226 | 0x00000000 | 0x00000000 | No
available to customer | OTP227 | 0x00000000 | 0x00000000 | No
available to customer | OTP228 | 0x00000000 | 0x00000000 | No
available to customer | OTP229 | 0x00000000 | 0x00000000 | No
available to customer | OTP230 | 0x00000000 | 0x00000000 | No
available to customer | OTP231 | 0x00000000 | 0x00000000 | No
available to customer | OTP232 | 0x00000000 | 0x00000000 | No
available to customer | OTP233 | 0x00000000 | 0x00000000 | No
available to customer | OTP234 | 0x00000000 | 0x00000000 | No
available to customer | OTP235 | 0x00000000 | 0x00000000 | No
available to customer | OTP236 | 0x00000000 | 0x00000000 | No
available to customer | OTP237 | 0x00000000 | 0x00000000 | No
available to customer | OTP238 | 0x00000000 | 0x00000000 | No
available to customer | OTP239 | 0x00000000 | 0x00000000 | No
available to customer | OTP240 | 0x00000000 | 0x00000000 | No
available to customer | OTP241 | 0x00000000 | 0x00000000 | No
available to customer | OTP242 | 0x00000000 | 0x00000000 | No
available to customer | OTP243 | 0x00000000 | 0x00000000 | No
available to customer | OTP244 | 0x00000000 | 0x00000000 | No
available to customer | OTP245 | 0x00000000 | 0x00000000 | No
available to customer | OTP246 | 0x00000000 | 0x00000000 | No
available to customer | OTP247 | 0x00000000 | 0x00000000 | No
available to customer | OTP248 | 0x00000000 | 0x00000000 | No
available to customer | OTP249 | 0x00000000 | 0x00000000 | No
available to customer | OTP250 | 0x00000000 | 0x00000000 | No
available to customer | OTP251 | 0x00000000 | 0x00000000 | No
available to customer | OTP252 | 0x00000000 | 0x00000000 | No
available to customer | OTP253 | 0x00000000 | 0x00000000 | No
available to customer | OTP254 | 0x00000000 | 0x00000000 | No
available to customer | OTP255 | 0x00000000 | 0x00000000 | No
OTP_RMA_LOCK_PSWD0 | OTP256 | 0x00000000 | 0x00000000 | No
OTP_RMA_LOCK_PSWD1 | OTP257 | 0x00000000 | 0x00000000 | No
OTP_RMA_LOCK_PSWD2 | OTP258 | 0x00000000 | 0x00000000 | No
OTP_RMA_LOCK_PSWD3 | OTP259 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP260 | 0xC48FFC64 | 0x40000000 | Yes
OEM Secrets available to customer | OTP261 | 0x8B94A062 | 0x40000000 | Yes
OEM Secrets available to customer | OTP262 | 0x0B9085FE | 0x40000000 | Yes
OEM Secrets available to customer | OTP263 | 0x68B30CC5 | 0x40000000 | Yes
OEM Secrets available to customer | OTP264 | 0x33E0B6E5 | 0x40000000 | Yes
OEM Secrets available to customer | OTP265 | 0xE30D255E | 0x40000000 | Yes
OEM Secrets available to customer | OTP266 | 0xD49FDEC8 | 0x40000000 | Yes
OEM Secrets available to customer | OTP267 | 0xBEE6EC4C | 0x40000000 | Yes
OEM Secrets available to customer | OTP268 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP269 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP270 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP271 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP272 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP273 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP274 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP275 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP276 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP277 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP278 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP279 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP280 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP281 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP282 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP283 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP284 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP285 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP286 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP287 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP288 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP289 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP290 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP291 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP292 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP293 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP294 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP295 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP296 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP297 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP298 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP299 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP300 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP301 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP302 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP303 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP304 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP305 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP306 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP307 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP308 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP309 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP310 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP311 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP312 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP313 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP314 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP315 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP316 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP317 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP318 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP319 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP320 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP321 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP322 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP323 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP324 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP325 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP326 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP327 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP328 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP329 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP330 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP331 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP332 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP333 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP334 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP335 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP336 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP337 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP338 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP339 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP340 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP341 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP342 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP343 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP344 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP345 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP346 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP347 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP348 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP349 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP350 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP351 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP352 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP353 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP354 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP355 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP356 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP357 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP358 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP359 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP360 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP361 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP362 | 0x00000000 | 0x00000000 | No
OEM Secrets available to customer | OTP363 | 0x00000000 | 0x00000000 | No
OEM_SECRET_FOR_CRYPTED_BOOT0 | OTP364 | 0x00000000 | 0x00000000 | No
OEM_SECRET_FOR_CRYPTED_BOOT1 | OTP365 | 0x00000000 | 0x00000000 | No
OEM_SECRET_FOR_CRYPTED_BOOT2 | OTP366 | 0x00000000 | 0x00000000 | No
OEM_SECRET_FOR_CRYPTED_BOOT3 | OTP367 | 0x00000000 | 0x00000000 | No
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Ok, so I got it working, the problem was that even when running the XSPI flash at 50 MHz the "high speed IO optimizations" should be enabled - see also this thread.
Thanks again @B.Montanari !
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Thank you @B.Montanari and ST team for the great article!
Do you have an example that checks the integrity of the Appli signature on the FSBL?
For example what happens if an error occurred during the copy?
The FSBL should be able to recover this and try again. As a first step it could check that the hash of the file in RAM matches that which was expected in the Header.
Looking through the LoadAndRun example it appears the Appli signature is ignored?
It appears the Application is copied from external flash to RAM, and then immediately executed, without checking its integrity?
Thank you again for the write up!
Kind regards,
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi @exarian , thanks for the feedback!
Please see my comments below:
Q1: Do you have an example that checks the integrity of the Appli signature on the FSBL?
C1: Currently we don't have any examples to cover that portion without using the Secure framework. Given the higher complexity of the topic, it will be addressed in our wiki page instead. The content is under creation, but will be here once available> Category:STM32N6 - stm32mcu
Q2: For example what happens if an error occurred during the copy?
C2: If an error happens during the copy, since there is no control or verification, it will execute the jump to the copied region and eventually get a hardfault.
Q3: Looking through the LoadAndRun example it appears the Appli signature is ignored?
C3: Yes, the Appli signature is ignored in this example, the firmware is bypassing/ignoring the header.
Q4: It appears the Application is copied from external flash to RAM, and then immediately executed, without checking its integrity?
C4: Correct, we can work on a code example that implements a small verification to ensure the copy is properly made.
Thanks!
Best Regards
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Thank you @B.Montanari ,
I really appreciate that feedback and your answers.
I will keep an eye on the Wiki's. I am excited to see what comes next, looking forward to future updates!
Kind Regards,
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi @asdfasdf ,
I've checked the board and chip review, you have the rev. B, which is the latest one so you are good on that portion, but checking the OTP dump, this one caught my attention:
BOOTROM_CONFIG_1 | OTP10 | 0x00030103
The bits 16 and 17 set in yours, but I st_pub_key_id, bits 15..18 are 0 as default. Not sure why those are set, security is not my area of expertise, but I believe this could be the root cause. If that is indeed the case, you should be able to use the simplified Load and Run, where the debugger loads the code directly in RAM memory and executes from there, while the board is in DEV mode, but the boot ROM would fail to copy from the external memory and load it into AXISRAM2 to get to the FSBL portion.
My suggestion is to issue a ticket on the online support, or reach out to your local FAE, asking it to be escalated to the security team, so they can comment on what can be done> OLS
Best Regards
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello, are there any updates on this?
It looks like i have the same problem. (Project basic settings: FSBL + Secure Only, XIP profile, 50Mhz XSPI -> just to be on the safe side). In fact, i went ahead to verify the inability to load FSBL from EXTMEM to RAM with multiple methods
a) I verified the contents of the EXTMEM for the first 64k @0x70000000 and at 0x70100000 and found it to be the same as fsbl & appli signed binaries so, the code is uploaded correctly, there is no degradation or failure of any kind
b) after flashing appli with programmer i uploaded in devmode though CubeIDE the FSBL binary only. The code started to run (jumped to 0x70100000 that had a led blinking code), so the appli code is capable of running correctly but is never called by FSBL. However, if FSBL is manualy loaded to RAM the appli code is called and run correctly!
That led me to the conclusion that for some reason the FSBL code @ 70000000 is not copied and run from memory!
I also have the same BOOTROM_CONFIG_1 | OTP10 | 0x00030103 value and there is no description for it at UM3234, thus, I’m now stuck unable to use the board for large ML models (>4.2MB) {although I can trick it by uploading the -large- appli and then the FSBL in DevMode}, this trick however may or may not affect some efficiency {power & latency} measurements I need to take.
I can make a new post for attaching the files or send the full project (.ioc + code) and the full otp export file if you need.
Can you please help?
Thanks.
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Thank you @Unfgr, your temporary trick works for me.
But is there any benefit for doing this trick compared to using CubeIDE's "Run As .." to directly program the Appli in Dev Boot?
- Mark as Read
- Mark as New
- Bookmark
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi @B.Montanari - thank you for the thorough example, I was able to get it running successfully on the DK.
I saw in the post that the flash memory is 1.8V but did not see any configuration anywhere of the IO bank/port to operate at 1.8V instead of 3.3V. Will I be damaging my DK (or my custom hardware based on the DK schematic) if I don't configure the OTP fuses and power control register (VDDIO2) for 1.8V operation?
Thank you!
Edit: I figured it out: I see that the DK board is pre-configured for 1.8V operation. I used CubeProgrammer to connect via ST-Link and examine the OTP bit/fuse values, and saw that HSLV_VDDIO2 and HSLV_VDDIO3 are already set to 1 to enable 1.8V operation.