cancel
Showing results for 
Search instead for 
Did you mean: 

How to change STM32CubeIDE to dark theme

B.Montanari
ST Employee

If you want a customized interface to work on your projects, you can try the alternatives offered by the STM32CubeIDE to personalize the appearance of your files.
To change the default settings to give it a personal touch, follow the steps below.

Create your project as usual >  click on Window > Preferences > General > Appearance > Theme > Choose between “Classic/ Dark / Light / System” themes
273.png
274.png
As you can see, if you want to, you can also change the settings for the color and font theme and, if you like round tabs, just activate the checkbox.
275.png
Notice that a warning appears when you change the theme settings, asking you to restart the program so your changes can take full effect.
Click apply, and let the program restart itself, as you will see in the next steps.
After that, you will have your STM32CubeIDE running in a dark theme mode.
With a few steps more, you can enjoy your new customized workspace.  
276.png277.png
As you can see, after the restart, some lines are not highlighted as they were in the light theme.  
You can change these settings going to Window > Preferences > General > Editors > Text Editors > Annotations.
Select the annotation types that you would like to change (“Search” was used as an example) and choose the color that fits you better.
278.png
To change the compiler background colors, if you wish, go to Window > Preferences > C/C++ > Build > Console
279.png
To finalize, you can also change the comment lines color going to Window > Preferences > C/C++ > Editor > Syntax Coloring > Comments
In the same path, you can change the color of other regions of your project–such as structs, typedefs, macros etc., in the “Code” option, as follows.
280.png
Hope you enjoy your new STM32CubeIDE personalized interface!
 

Comments
Ahmet Yasin CİVAN
Associate III

Thank you for sharing.

志肖.1
Associate II

Thank you very much.

SGran.5
Associate II

can set: Dark-Reduced Palette onli for main.c or othe .c files ; separately from each other - together these files have a different color - this appeared after the update

STM32CubeIDE

Version: 1.12.1

Build: 16088_20230420_1057 (UTC)

Christina_L
Associate

STM32CubeIDE 1.16.1 (macOS)

Click on STM32CubeIDE >> Settings >> General >> Appearance, then select Dark Theme

Version history
Last update:
‎2024-06-18 1:05 AM
Updated by:
Contributors