cancel
Showing results for 
Search instead for 
Did you mean: 

Zephyr support for nucleo-wb15cc

StevenG
Associate III

Is support for the nucleo-wb15cc already in Zephyr or does it need to be added?  I am new to zephyr and would like to avoid re-inventing the wheel if possible.

 

From a setup I just created today (so should have the latest released code) I didn't see the wb15 listed:

(.venv) g:~/zephyrproject/zephyr$ west boards | grep -i -e stm32 -e nucleo | grep -i wb
nucleo_wba55cg
nucleo_wb05kz
stm32wb5mm_dk
nucleo_wb09ke
stm32wb5mmg
nucleo_wb55rg
nucleo_wba52cg

1 REPLY 1
Saket_Om
ST Employee

Hello @StevenG 

These boards are not supported today; you will need to add them.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om