cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-WB05KN1 - Zephyr Problem

CBras
Associate II

Hi,

I have attached a X-NUCLEO-WB05KN1 on top of a NUCLEO-H743ZI2 board and are trying to verify whether it works by flashing the peripheral_hr sample with the shield argument "x_nucleo_wb05kn1_spi". Sadly it does not work (it is stuck in bt_spi_open when trying to receive SPI header from shield)

The shield is flashed such that it uses SPI instead of UART.

I have done the same experiment, placing the shield on top of Nordic Semiconductors' nRF52840 MCU and here it works with the peripheral_hr sample with shield argument.

I have also tried the experiment on a NUCLEO-F401RE and here it also fails.

Any ideas what could be wrong?

4 REPLIES 4
CBras
Associate II

Any updates?

STTwo-32
ST Employee

Hello @CBras 

This behavior has been escalated internally (under internal ticket number 208694). I will get back to you ASAP.

Best Regards.

STTwo-32  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

dd1337
Associate

I'm experiencing the same issue

CBras
Associate II

I was handed a temporary solution almost a month ago but it doesn't seem like the right fix has been provided to upstream zephyr.. I have attached the file.