2021-08-04 07:47 AM
I am trying to setup UART1 on WL55CC; using RTS;
#include <stdio.h>
#if defined (__ICCARM__) || defined (__ARMCC_VERSION)
#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
#elif defined(__GNUC__)
/* With GCC, small printf (option LD Linker->Libraries->Small printf
set to 'Yes') calls __io_putchar() */
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#endif /* __ICCARM__ || __ARMCC_VERSION */
HAL_GPIO_TogglePin(GPIOA, LED_Pin); // PORTA, PA9
HAL_Delay(500);
nLoop++;
printf("nLoop == %d \n\r", (int) nLoop);
PUTCHAR_PROTOTYPE
{
/* Place your implementation of fputc here */
/* e.g. write a character to the USART1 and Loop until the end of transmission */
HAL_UART_Transmit(&huart1, (uint8_t *)&ch, 1, 0xFFFF);
return ch;
}
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_RTS;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
extern int __io_putchar(int ch) __attribute__((weak));
extern int __io_getchar(void) __attribute__((weak));
I might not be linking tiny printf, but I don't know where that is.
Please help
2021-08-04 08:14 AM
If you call HAL_UART_Transmit from multiple contexts, the ones that are called later will return HAL_BUSY if a call is already ongoing. It doesn't look like HAL_BUSY can be called due to RTS, but I could be wrong here.
You can implement your own buffer, disable interrupts during the call, or just ignore the lost bytes. It calls HAL_Delay, but I do not think disabling interrupts will prevent normal operation in this case.