cancel
Showing results for 
Search instead for 
Did you mean: 

Which EVK should be used for STM32WB55CG.

PMana.1
Associate II

I am working on a lorawan project targeted at STM32WB55CGT6. It is QFN48 and I tried running the successful project on NUCLEO-WB55CG. The development board is QFN64. Would I be able to use the same Nucleo board for further development for STM32WB55CGT6? In addition, what is the difference between P-NUCLEO-WB55CG and NUCLEO-WB55CG? Please suggest to me the best evk for STM32WB55CGT6.

Thanks in advance

2 REPLIES 2
Bruno_ST
ST Employee

Hello @PMana.1​ 

Lorawan device is supported by default on STM32WL not on STM32WB (BLE). There is 2 version of the nucleo board depending of the targeted frequency (433MHz/868MHz).

Is you project trying the LoRa @ 2.4GHz ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi, I am using LR1110 and I need bluetooth too. so the chip is stm32wb55. I can't make change on the mcu selected. I just want to know, which development board should I use.. Thanks