cancel
Showing results for 
Search instead for 
Did you mean: 

What firmware to flash so the STM32WB board can be used with CubeMonitor-RF

RSchm
Associate

I have got an STM32WB55 DK and i would like to use it with the CubeMonitor-RF.

I flashed the image for the co-processor but i am not sure which firmware for the main processor. I flashed the BLE Transparent Mode Application Firmware but the CubeMonitor-RF can not connect to the UART.

Thanks for your support!

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

It May be caused by failure in memory recognition system in CubeProg (​if it's based on serial or other number hardcoded in bootloader)

Is it possible to flash radio binary via SWD?

I have holidays, so I can check it after week. ​

I've tried and it failed. Also my dongle is recognized in Device Manager.

During stack upgrade 256 kiBytes of memory are shown.

USB Dongles have 1MiB

Log below:

     -------------------------------------------------------------------

                      STM32CubeProgrammer v2.1.0

     -------------------------------------------------------------------

USB speed  : Full Speed (12MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : DFU in FS Mode

SN         : 205E38773036

FW version : 0x011a

Device ID  : 0x0495

Device name : STM32WBxx

Flash size : 256 KBytes

Device type : MCU

Device CPU : Cortex-M0+/M4

Download firmware image at address 0x80cc000 ...

Memory Programming ...

Opening and parsing file: stm32wb5x_BLE_Stack_fw.bin

 File         : stm32wb5x_BLE_Stack_fw.bin

 Size         : 162908 Bytes

 Address      : 0x080CC000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [204 243]

Download in Progress:

██████████████████████████████████████████████████ 100%

File download complete

Time elapsed during download operation: 00:00:01.765

Verifying ...

Read progress:

██████████████████████████████████████████████████ 100%

Download verified successfully

RSS state is RSS_SERVICE_ONGOING

RSS status is RSS_IMAGE_NOT_FOUND

RSS state is RSS_IDLE

RSS status is RSS_NO_ERROR

Firmware Upgrade process started ...

Updating firmware ...

Waiting for firmware upgrade end

RSS state is WIRELESS_STACK_UPGRADE_ONGOING

RSS status is RSS_IMAGE_NOT_FOUND

Warning: Firmware upgrade Error!Retrying...

Retry -- 0

etc.