I've tried and it failed. Also my dongle is recognized in Device Manager. During stack upgrade 256 kiBytes of memory are shown.USB Dongles have 1MiBLog below: ------------------------------------------------------------------- ...
It May be caused by failure in memory recognition system in CubeProg (if it's based on serial or other number hardcoded in bootloader)Is it possible to flash radio binary via SWD?I have holidays, so I can check it after week.
I have the same problem, moreover my device was recognized as 256kB variant, not as 1MB. Something is wrong with these dongles, or with firmware?I've updated FUS to newest version