2025-04-03 12:08 AM
Hello,
CFG_BONDING_MODE and CFG_FIXED_PIN are not correctly generated and CFG_FIXED_PIN is updated only when IO capability is changed:
and this is content of app_conf.h:
CFG_BONDING_MODE and CFG_USED_FIXED_PIN are always set to 1.
Best regards
Solved! Go to Solution.
2025-04-03 1:33 AM
Hello @cvs_dk
I'm not able to reproduce this behavior using the STM32CubeIDE V1.18.0, STM32CubeMX V6.14.0 and the STM32CubeWBA V1.6.0. It may be an issue on an old version that has been solved. So, I suggest you update and start using the last versions.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-03 1:33 AM
Hello @cvs_dk
I'm not able to reproduce this behavior using the STM32CubeIDE V1.18.0, STM32CubeMX V6.14.0 and the STM32CubeWBA V1.6.0. It may be an issue on an old version that has been solved. So, I suggest you update and start using the last versions.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.