2019-08-23 5:08 AM
i'm trying to use the Nucleo WB55 dongle as a mass storage device.
Using cubeMx i set the USB, and the USB Middleware as MSC, leaving the default settings. Nothing else is running on the dongle, just USB.
When i plug it, it appear as an unknown device. Windows is returning an Error 43 Code [
43 (CM_PROB_FAILED_POST_START)]
Uppon connection, USB events are as follow:
000000: PnP Event: Device Connected (UP), 2019-08-23 11:07:13,0401325 (1. Device: Unknown)
The USB device has just been connected to the system.
000001: PnP Event: Surprise Removal (UP), 2019-08-23 11:07:13,0411870 +0,0010545 (1. Device: Unknown)
The USB device has just been disconnected from the system.
000002: PnP Event: Device Disconnected (UP), 2019-08-23 11:07:13,0413300 +0,0001430 (1. Device: Unknown)
The USB device has just been removed from the system, all drivers unloaded
Using debug, i checked that nothing was skipped, and i also add printf messages through SWO to be sure that all the USB init is done properly. And also to check what happen once the interrupt is enabled in USBD_Start().
The following is the start of the SWO message, showing that all the MX_USB_Device_Init() is done without error, and showing the function call made in HAL_PCD_IRQHandler().
USBD_Init returned USBD_OK @ 1 ms
USBD_RegisterClass returned USBD_OK @ 1 ms
USBD_MSC_RegisterStorage returned USBD_OK @ 2 ms
0 - HAL_PCD_ResetCallback @ 3 ms
1 - HAL_PCD_SetAddress @ 3 ms
USBD_Start returned USBD_OK @ 4 ms
2 - HAL_PCD_SuspendCallback @ 6 ms
3 - HAL_PCD_ResumeCallback @ 104 ms
4 - HAL_PCD_ResetCallback @ 158 ms
5 - HAL_PCD_SetAddress @ 158 ms
6 - HAL_PCD_SOFCallback @ 158 ms
7 - HAL_PCD_SOFCallback @ 159 ms
8 - HAL_PCD_SOFCallback @ 160 ms
9 - HAL_PCD_SOFCallback @ 161 ms
10 - HAL_PCD_SOFCallback @ 162 ms
11 - HAL_PCD_SOFCallback @ 163 ms
12 - HAL_PCD_SOFCallback @ 164 ms
13 - HAL_PCD_SOFCallback @ 165 ms
14 - HAL_PCD_SOFCallback @ 166 ms
15 - HAL_PCD_SOFCallback @ 167 ms
16 - HAL_PCD_SOFCallback @ 168 ms
17 - HAL_PCD_SOFCallback @ 169 ms
18 - HAL_PCD_SOFCallback @ 170 ms
19 - HAL_PCD_SOFCallback @ 171 ms
the HAL_PCD_IRQHandler() call several functions (mostly the SOFcallback) for 2150ms.
I tried that on different computer, on W10 & W7.
And the strangest part is: it work on my own computer (W7).
My own computer is the only one where the USB is working fine.
I don't understand why. On every computer i checked the drivers, nothing wrong.
I don't need an external pull up, and the DPPU bit that turn on the pullup is called and work as expected. DP/DM are not swapped (even though it's an STM product i checked to be sure)
Vbus is perfect, and to be safe i also add a small delay before the USB Init.
I created different project, using different settings, but still error 43.
I don't know what could cause that issue and at that point i think i tried everything.
That issue is above my knowledges.
So if you have any idea, feel free to give your opinion.
Romain
Solved! Go to Solution.
2019-08-23 5:51 AM
dear @rcard,
Even if it is not a direct response to your question, i stronlgy recommend you to start with a working environment before trying to move to a from scratch solution.
The STM32Cube_FW_WB_V1.2.0 contains 2 applications to demonstrate the USB application on the P-NUCLEO-WB55.USBDongle and 4 USB applications on P-NUCLEO-WB55.Nucleo.
It is not MSC but HID and DFU for P-NUCLEO-WB55.USBDongle.
On the P-NUCLEO-WB55.Nucleo, you can have your exact setup: MSC (Warning: This application requires a separated shield (Adafruit 1.8" TFT shield) to embeded an sd card!).
USB_Device
CDC_Standalone (P-NUCLEO-WB55.Nucleo)
DFU_Standalone (P-NUCLEO-WB55.Nucleo and P-NUCLEO-WB55.USBDongle)
HID_Standalone (P-NUCLEO-WB55.Nucleo and P-NUCLEO-WB55.USBDongle)
MSC_Standalone (P-NUCLEO-WB55.Nucleo)
Those example are created with STM32CubeMX so you can check which part is missing on your environment.
They can be found under :
I just test on my laptop Win10 P-NUCLEO-WB55.USBDongle with HID_Standalone and P-NUCLEO-WB55.Nucleo with MSC_Standalone (be sure to have the Adafruit 1.8" TFT shield and a sd card) and they behave as expected to demonstrate the USB device mode of STM32WB55xx.
BR.
Pierre.
2019-08-23 5:51 AM
dear @rcard,
Even if it is not a direct response to your question, i stronlgy recommend you to start with a working environment before trying to move to a from scratch solution.
The STM32Cube_FW_WB_V1.2.0 contains 2 applications to demonstrate the USB application on the P-NUCLEO-WB55.USBDongle and 4 USB applications on P-NUCLEO-WB55.Nucleo.
It is not MSC but HID and DFU for P-NUCLEO-WB55.USBDongle.
On the P-NUCLEO-WB55.Nucleo, you can have your exact setup: MSC (Warning: This application requires a separated shield (Adafruit 1.8" TFT shield) to embeded an sd card!).
USB_Device
CDC_Standalone (P-NUCLEO-WB55.Nucleo)
DFU_Standalone (P-NUCLEO-WB55.Nucleo and P-NUCLEO-WB55.USBDongle)
HID_Standalone (P-NUCLEO-WB55.Nucleo and P-NUCLEO-WB55.USBDongle)
MSC_Standalone (P-NUCLEO-WB55.Nucleo)
Those example are created with STM32CubeMX so you can check which part is missing on your environment.
They can be found under :
I just test on my laptop Win10 P-NUCLEO-WB55.USBDongle with HID_Standalone and P-NUCLEO-WB55.Nucleo with MSC_Standalone (be sure to have the Adafruit 1.8" TFT shield and a sd card) and they behave as expected to demonstrate the USB device mode of STM32WB55xx.
BR.
Pierre.
2019-08-25 10:45 PM
Hello,
Thanks for your answer. I'm going to try that and see if i can finally run USB without the error code 43.
Romain
2019-08-26 2:42 AM
Ok so the applications seems to work fine. So now i need to find where my error is, and what i have made differently.
Thanks again, i never though of ST's example .
Romain
2019-08-27 11:40 PM
So, to give an update on this issue:
I modified the MSC Standalone for the NucleoWB55 (not the dongle) to use the SRAM instead of a SD card (because i don't have the adafruit shield). And boom it worked. I now have a working MSC App.
The thing is i still don't understand why. I followed ST's youtube video to setup the USB MSC, and it didn't work. But for some reason the ST App is running fine.
The only thing i can think of is the clock. In my app i used the 32MHz HSE to clock the USB. I should have tried with the internal RC. Even though it's not that logical.
Now i will try to transfer the code from the STM32WB55RG to the STM32WB55CC and see if i can still having it to work.
2019-08-28 12:46 AM
Ok so i have transferred file by file the working project to the non working project, and i narrowed the faulty part to be in the usbd_desc.c file.
I can't find my error, but copying the MSC_Standalone usbd_desc.c file to my project solved the issue. I guess at some point in the setting i made a mistake.
Thanks again @Le Corre Pierre without you i would not have though of the ST's application.
Have a good day.
Romain