UART trames are not good
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-06 1:21 AM
Hello I am worcking an the P-NUCLEO-WB55 and I try to communicate with a other module with the LPUART. Seeing that I didn't have any responce to my commands, I use a scope to see the TX trame.
This is for example the trame of '<' (00111100) .
I used the command HAL_UART_Transmit(&hlpuart1, '<', 1, HAL_MAX_DELAY);
And there, the LPUART parameters:
static void MX_LPUART1_UART_Init(void)
{
/* USER CODE BEGIN LPUART1_Init 0 */
/* USER CODE END LPUART1_Init 0 */
/* USER CODE BEGIN LPUART1_Init 1 */
/* USER CODE END LPUART1_Init 1 */
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = 115200;
hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart1.Init.StopBits = UART_STOPBITS_1;
hlpuart1.Init.Parity = UART_PARITY_NONE;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
hlpuart1.FifoMode = UART_FIFOMODE_DISABLE;
if (HAL_UART_Init(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN LPUART1_Init 2 */
/* USER CODE END LPUART1_Init 2 */
}
I tired to send many other caracters but I never see the good trame on the scope.
Any idea of what appened?
- Labels:
-
STM32WB series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-06 1:30 AM
I think HAL_UART_Transmit needs a C string "<" not a single character '<'.
Hope this helps,
Danish
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-06 2:18 AM
Well not really but thanks for the advice
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-06 4:22 AM
You might have some other things wrong, but when you call
HAL_UART_Transmit(&hlpuart1, '<', 1, HAL_MAX_DELAY);
what the library-function is expecting is of the form
HAL_StatusTypeDef HAL_UART_Transmit(UART_HandleTypeDef *huart, uint8_t *pData, uint16_t Size, uint32_t Timeout);
So you are giving '<' to the pointer-to-string variable pData.
What does the C compiler do under these circumstances?
It gets the ascii value of the character '<', in this case 0b00111100 or 0x3c
And passes that as the address for where to find the (in your case one-character) string.
And then the library-function then sends whatever happens to be in memory location 0x3c. Not the value 0x3c.
If instead you did
HAL_UART_Transmit(&hlpuart1, "<", 1, HAL_MAX_DELAY);
The C compiler would create a C string consisting of your character '<' and the string-terminator '\0' and store it in program memory. It would pass the address of that string to HAL_UART_Transmit(). And the library-function would look in the memory-location specified by the address, and retrieve the character '<' and send it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-06 4:23 AM
@Danish​ is correct: you are sending over UART what's at 0x0000003c address, not the actual '<' character.