cancel
Showing results for 
Search instead for 
Did you mean: 

Non standard preamble on STM32WL33

DirkH
Associate II

I need to implement a protocol using 11110000 as preamble. The protocol is 2-FSK 868.1 MHz, +/-35kHz, 25kbps. According to RM0511 STM32WL33 only supports 01010101 or 10101010 as preamble for 2-FSK. Is it feasible to use the STM32WL33? I am planning to use direct buffer mode.

1 ACCEPTED SOLUTION

Accepted Solutions
Filippo_Malleo
ST Employee

Hi DirkH, 

yes, you can use the Direct through buffer mode, so you can implement your protocol bypassing any packet handler constraint.

BR,
Filippo

View solution in original post

1 REPLY 1
Filippo_Malleo
ST Employee

Hi DirkH, 

yes, you can use the Direct through buffer mode, so you can implement your protocol bypassing any packet handler constraint.

BR,
Filippo

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.