SUBSTITUTION LORA GATEWAY WITH A STM32-L476RG
Hi everyone, i would create a LoRaWAN project in which both end-node and gateway are implemented by a NUCLEO-l476rg, because i haven't a gateway. The fictitous gateway is connected locally, with UART, to a python app on my pc, to handle the information trasmetted by the endnode. I have implemented both sides: 1) endnode, with a LoRaWAN endnode example from STM32CubeExpansion_LRWAN, 2) the gateway's programm is a modificated pingping example, to receive and forward then to python.
My problem is: premising that I set the tx frequency always to the first channel(868100000) when the end-node transmit, the "gateway doesn't receive every time, as well as is showed in this log:
16s627:Packet received
26s627:Packet received
36s627:Packet received
56s627:Packet received
66s627:Packet received
96s627:Packet received
106s627:Packet received
The gateway should receive a packet every 10 s, but this doesn't happend. Someone can tell my why?