cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WPAN stops advertising after registering custom task

KlemenPfce
Associate III

I have a application where stm32wb5mm is acting like a beacon. I got it to advertise configured data, now I am trying to advertise temperature measurement, for this, I need to dynamically update advertising data packages.

 

So my advertising works ok, when it is just the template:

/* Initialize all configured peripherals */ MX_RF_Init(); MX_GPIO_Init(); MX_RTC_Init(); MX_I2C3_Init(); /* USER CODE BEGIN 2 */ //UTIL_SEQ_RegTask((1 << 0), 0, task2); /* USER CODE END 2 */ /* Init code for STM32_WPAN */ MX_APPE_Init(); /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { //UTIL_SEQ_SetTask((1 << 0), 0); /* USER CODE END WHILE */ MX_APPE_Process(); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ }

But as soon as I enable the task that i created, the advertising stops:

/* Initialize all configured peripherals */ MX_RF_Init(); MX_GPIO_Init(); MX_RTC_Init(); MX_I2C3_Init(); /* USER CODE BEGIN 2 */ UTIL_SEQ_RegTask((1 << 0), 0, task2); /* USER CODE END 2 */ /* Init code for STM32_WPAN */ MX_APPE_Init(); /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { UTIL_SEQ_SetTask((1 << 0), 0); /* USER CODE END WHILE */ MX_APPE_Process(); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ }

 

Content of registered task:

{ a_AdvData[23] = update_data(); //gets temperature data and stores in adv struct aci_gap_update_adv_data(sizeof(a_AdvData), (uint8_t*) a_AdvData); //Update adv data }
1 ACCEPTED SOLUTION

Accepted Solutions
KlemenPfce
Associate III

Found solution, problem was that ID that I used for my custom task registration, was already taken by CubeMX configured firmware. Changed to task ID to "2", now works without a hitch.

View solution in original post

1 REPLY 1
KlemenPfce
Associate III

Found solution, problem was that ID that I used for my custom task registration, was already taken by CubeMX configured firmware. Changed to task ID to "2", now works without a hitch.