cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WL55 subghz radio low level hardware init for a custom board

pavitrar
Associate

I am trying to test the SUB GHZ interface on STM32WL5xxU7. Is there any starter code without reliance on Nucleo boards that I could use to start with? Or are there steps how to do this with Low level drivers  ? 

1 REPLY 1
STTwo-32
ST Employee

Hello @pavitrar and welcome to the ST Community 😊.

The examples that we are developing are tested using our evaluation boards. But, you can try to adapt them to your own board. That should be easy to do. For the steps on how to do this with Low level drivers, you can refer to a good tutorial on this link.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.